imx535 LPDDR2 Connection, any help?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx535 LPDDR2 Connection, any help?

2,386件の閲覧回数
danix
Contributor III

Hey all,

I know I'm posting this for the third time, but I need to make sure connecting micron 4Gb LPDDR2

with imx535(529-BGA). I'm stuck here...

The DDR has multiplexed command/address line CA[9:0]... how am I going to connect this to the DDR controler in mx53?

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,126件の閲覧回数
danix
Contributor III

Aven,

Thank you for your reply. The address and data connection is is not a concern; It's a little obvious, don you think?

 I was rather concerned about the power supply. The LPDDR2 needs two different levels, 1.2V and 1.8V and the datasheet suggested the 1.8V be ramped first. Using the  MC34708 PMIC, how I'm I going to do that and which source should be used for the 1.8V?

PS: I'm using the Micron MT42L128M32D2: 4Gb, LPDDR2  PoP

0 件の賞賛
返信

2,126件の閲覧回数
aven_tsao
NXP Employee
NXP Employee

Sorry for my mistake, please connect CA[9:0] to MX53 DRAM_A[9:0]

Aven

0 件の賞賛
返信

2,126件の閲覧回数
aven_tsao
NXP Employee
NXP Employee

Dear Sir:

Since the DRAM Address bus are used for Address and Command transfer.

So, please connect CA[9:0] to MX53 DRAM[9:0]

Aven Tsao

0 件の賞賛
返信