imx53 quick start board development environment

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx53 quick start board development environment

ソリューションへジャンプ
21,208件の閲覧回数
leonardfairclot
Contributor II

I'm stepping through the steps and here are a few issues that I have found:  Please note I'm working with Ubuntu:

7.3.5 - Configure tftp server

               I do not have "/etc/inetd.conf" or "/etc.default/atftpd".  I also do not have "/etc/exports" is this a new file?

Do I need this to compile code for the imx53?

I skipped this and continued on and then ran into:

"user@ubuntu:~/imx53/11.09.01/L2.6.35_11.09.01_ER_source$ ls

EULA  install  ltib.tar.gz  package_manifest.txt  pkgs  redboot_201003.zip  tftp.zip"

"~/imx53/11.09.01/L2.6.35_11.09.01_ER_source$" directory of file does not exist, if I take the $ off it says this is a directory.  What is this looking for?  This is a directory but I'm not sure what it is looking for.

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
19,516件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please use the next topic how to prepare virtual machine for LTIB.

https://community.freescale.com/message/294343#294343

Please pay attention on files "Create-Ubuntu11-10-ltib11-09-01.docx" and  "ubuntu-ltib-patch.tgz", linked there.

I tried the described approach on Ubuntu 12.04 - it works.

元の投稿で解決策を見る

0 件の賞賛
返信
62 返答(返信)
19,517件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please use the next topic how to prepare virtual machine for LTIB.

https://community.freescale.com/message/294343#294343

Please pay attention on files "Create-Ubuntu11-10-ltib11-09-01.docx" and  "ubuntu-ltib-patch.tgz", linked there.

I tried the described approach on Ubuntu 12.04 - it works.

0 件の賞賛
返信
10,082件の閲覧回数
leonardfairclot
Contributor II

Yuri

Back at it again. I'm doing updates now but if youcould send me the

"Create-Ubuntu11-10-ltib11-09-01.docx" I would appreciate it. The link

isn't working.

Thanks

0 件の賞賛
返信
10,082件の閲覧回数
leonardfairclot
Contributor II

Yuri

Have you tried that link 'Create-Ubuntu11-10-ltib11-09-01.docx',

recently? I would like to see this doc but the link doesn't seem to

work.

Thanks

Leonard

0 件の賞賛
返信
10,078件の閲覧回数
Yuri
NXP Employee
NXP Employee

Enclosed.

0 件の賞賛
返信
10,078件の閲覧回数
leonardfairclot
Contributor II

Yuri

Not sure if you recieved my last email, I need

"ltib-fix-rpm-flag.patch". I cannot find it.

Thanks

Leonard

0 件の賞賛
返信
10,078件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please look at section

9.3.1Patch LTIB

of "Ubuntu 11.10 64-bit host  i.MX53 START_R LTIB 11.09.01 Installation"  - it contains the source.

0 件の賞賛
返信
10,078件の閲覧回数
leonardfairclot
Contributor II

Patch file attached, can you take a look before I run it?

thanks

Leonard

0 件の賞賛
返信
10,077件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please try the enclosed (in <ltib> directory)

patch -p 0 < ltib-fix-rpm-flag.patch

0 件の賞賛
返信
10,077件の閲覧回数
leonardfairclot
Contributor II

Yuri

It built successfully! very hapy about that. I was curious about other

develpers. How do they build and move to the imx53 board? Do they use

Putty? What language do they use, I was planning on using C. is there

a way to connect to a mysql database, like in windows you wold use odbc?

I tried calling on your skype, if you could i would like to talk to you

for a few minutes.

thanks

Leonard

0 件の賞賛
返信
10,077件の閲覧回数
Yuri
NXP Employee
NXP Employee

Leonard, good day !

> ... It built successfully!  ...


Great !

As for applications development, as has been mentioned in SR :
The following may be helpful.

AN3870 : Developing an Application for the i.MX Devices on Linux Platform

http://cache.freescale.com/files/dsp/doc/app_note/AN3870.pdf


The next app note may be useful in debugging :

"AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors."

http://cache.freescale.com/files/32bit/doc/app_note/AN4553.pdf

Regarding how to transfer an application (.elf, .bin) to i.MX53 board - at first 
it may be recommended to use NFS for debugging.


Also a SD card, USB sticker may serve in the same manner as for desktop PC.

We can use SCP to load and run codes to target Linux.


As for SQL - I am not a guru here - have not not tried it yet.

----

I am on-line.

0 件の賞賛
返信
10,077件の閲覧回数
leonardfairclot
Contributor II

Yuri

For the heck of it I tried:

/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/../lib/gcc/arm-fsl-linux-gnueabi/4.4.4/../../../../arm-fsl-linux-gnueabi/bin/gcc

-o HelloWorld.out HelloWorld.c

I recieved:

gcc: error trying to exec 'cc1': execvp: No such file or directory

Thanks again for you help

Leonard

0 件の賞賛
返信
10,077件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please use the next path :

/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/

and prefix : arm-fsl-linux-gnueabi-

So :

/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/arm-fsl-linux-gnueabi-gcc

-o HelloWorld.out HelloWorld.c

0 件の賞賛
返信
10,077件の閲覧回数
leonardfairclot
Contributor II

Here's my program:

#include <stdio.h>

int main()

{

printf("Hello World");

return 0;

}

execute

/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/arm-fsl-linux-gnueabi-gcc

-o HelloWorld.out HelloWorld.c

I get:

HelloWorld.c: In function 'main':

HelloWorld.c:6: error: stray '\302' in progress

HelloWorld.c:6: error: stray '\250' in progress

HelloWorld.c:6: error: 'hello' undeclared (first use in this function)

HelloWorld.c:6: error: (Each undeclared idnetifier is reported only

once)

HelloWorld.c:6: error: for each function it appears in.)

HelloWorld.c:6: error: expected ')' before 'World'

HelloWorld.c:6: error: stray '\302' in progress

HelloWorld.c:6: error: stray '\250' in progress

This should be pretty easy. What am I missing . I think I would be

better off uding Eclipse. I'll keep working on that.

Leonard

0 件の賞賛
返信
10,077件の閲覧回数
Yuri
NXP Employee
NXP Employee

Looks like some symbols are not in ASCII, say, text was prepared using Windows editor.

(Use Notepad++ in Windows). Also sequence "\n\r" in end of line (instead of '\n' for "true"
Linux ) may provide issues. 

0 件の賞賛
返信
10,077件の閲覧回数
leonardfairclot
Contributor II

Yuri

I posted the question on the community web site. Not sure what

happened, you were supposed to have a sample program for me and I don't

hear from you. I'm on a time crunch, I know it doesn't effect you but

it's huge for me. I've been at this for days and I can't compile a 4

line piece of code with the tools suggested by freescale. It shouldn't

be that difficult.

0 件の賞賛
返信
10,077件の閲覧回数
Yuri
NXP Employee
NXP Employee

The example (enclosed) was sent in SR# 1-1043955938.

The simplest way to compile an application  (say, "Hello World" example) is to use LTIB shell. To enter the shell  the next command may be applied :

<LTIB_DIR>/ltib -m shell

LTIB>

After that  proper environment for development is provided and code may be built as following :

LTIB> gcc -o hello.out hello.c

2.

Also please use the enclosed example (Makefile approach) how to configure environment in order to build an application under host Linux. 

0 件の賞賛
返信
10,077件の閲覧回数
leonardfairclot
Contributor II

Yuri

I complied it and copied it over to the imx53 board. I tried just using

the terminal and typing "hello" and it came back with "command not

found" I set the permission to the file and recieved the same results.

I tried to have it open with "Autorun Prompt" and the same results.

Leonard

0 件の賞賛
返信
10,077件の閲覧回数
Yuri
NXP Employee
NXP Employee

"command not found" means, that executable file hello was not found neither in (recent) default directory nor in directories,
mentioned in PATH environment. Please check if "hello"  application is located in current directory.
Another option - please apply "chmod 777 ./hello" command in the directory, where "hello" is located.
(hello should has executable attribute) 

0 件の賞賛
返信
10,077件の閲覧回数
leonardfairclot
Contributor II

Hi Yuri

Thanks, I was able to run HelloWorld! I'm installing QT and I'm at step

6, the only "qmake.conf" is under

"qtbase/mkspecs/devices/linux_imx6=g++/". Do I need to have a

"linux_imx5-g++" or go with the "6"? When it talks about copying and

pasting to a text file are they taling about a make file? I think I

better get this step correct or I'll be hating life on the next steps!

BTW: I'm changing my email address to "[email protected]", I'll

change it on my account tonight.

Thanks

Leonard

0 件の賞賛
返信
10,077件の閲覧回数
Yuri
NXP Employee
NXP Employee

Leonard, good day !

Please look at my comments below.


1.

> ... "qmake.conf" is under "qtbase/mkspecs/devices/linux_imx6=g++/". 
> Do I need to have a "linux_imx5-g++" or go with the "6"? 


"linux_imx5-g++

2.
> When it talks about copying and
pasting to a text file are they taling about a make file? 

Yes.

0 件の賞賛
返信