imx53 gpio interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx53 gpio interrupt

2,016件の閲覧回数
海罗
Contributor I

Now,I use kernal-2.6.35 with xenomai Patch and register a gpio(gpio2-14) interrupt,but when running the kernal  i find it always lose some response.

The time is interrupted every 500us ,some times it will lose three consecutive.  I don"t know why .The code:

#define MY_GPIO2_14   (1*32+14)

int irq = gpio_to_irq( MY_GPIO2_14);

.....................

.............................

int irq_handle_function(int irq, void *device_id)

{

disable_irq(irq);

if(phase==PH_RUNNING)

ctrl_mnm1221_m();

enable_irq(irq);

return IRQ_HANDLED;

}

......................................

.........................................

....................................

mxc_iomux_v3_setup_pad( MX53_PAD_PATA_DATA14__GPIO2_14 );
ret = gpio_request(MY_GPIO2_14, "RTEX" );
if( ret < 0 )
{
printk( KERN_ALERT"can not get irq,error!\n" );
}
gpio_direction_input( MY_GPIO2_14);

printk( KERN_ALERT"imxint_irq = %d\n", irq );
ret = request_irq( irq, irq_handle_function, IRQF_TRIGGER_LOW , "imx-int", NULL );
if( ret )
{
printk( KERN_ALERT"IRQ request failed!\n" );
gpio_free( MY_GPIO2_14 );
return ret;
}
gpio_free( MY_GPIO2_14 );

Is somewhere wrong ? Should  I  set the priorities of interruption? It need strong real-time requirements.  Thanks

タグ(3)
0 件の賞賛
返信
1 返信

1,186件の閲覧回数
9crkzhou
Contributor III

did your ever set the irq type? falling edge or rising edge?

0 件の賞賛
返信