imx53的IPU的两个通道就是指LVDS的两个通道么?要是我想两路LVDS和一路TTL上同时显示,但是IPU只有两个通道,这样可以实现么

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx53的IPU的两个通道就是指LVDS的两个通道么?要是我想两路LVDS和一路TTL上同时显示,但是IPU只有两个通道,这样可以实现么

跳至解决方案
977 次查看
wlwwlw
Contributor I

如标题

0 项奖励
回复
1 解答
771 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee

iMX53 IPU has two DI (Display interface) which can support two different displays, but for LVDS, if the two LVDS displays are same, they can connected two LVDS port but get data from same IPU DI, in this case, another display can be supported on another DI. The limitation for this use case: the two LVDS panels are same timing, same resolution, and show same content.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
771 次查看
YixingKong
Senior Contributor IV

Wlw, if your questions had been answered please clicking Correct Answer/Helpful Answer. We will close the Di if not response in 3 days.

Thanks,

Yixing

0 项奖励
回复
772 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee

iMX53 IPU has two DI (Display interface) which can support two different displays, but for LVDS, if the two LVDS displays are same, they can connected two LVDS port but get data from same IPU DI, in this case, another display can be supported on another DI. The limitation for this use case: the two LVDS panels are same timing, same resolution, and show same content.

0 项奖励
回复