imx51 usb_otg using for device mode errro

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx51 usb_otg using for device mode errro

跳至解决方案
3,285 次查看
shenjin
Contributor II

Hi,

when the imx515 otg interface to be using as a host mode,it is working well. in this mode,the pin ID is connect to ground.

now ,I want to use this interface as a OTG function, when we let the  ID pin floating,our kernel running erro,stop on the bleow message.

this issue was reproduce on the imx515 evk board also. who  can  help me ?

 

regulator_init_complete: disabling VVIDEO

regulator_init_complete: disabling VSD

regulator_init_complete: disabling VDIG

drivers/rtc/hctosys.c: unable to open rtc device (rtc0)

mmc0: new SDHC card at address fdfd

mmcblk0: mmc0:fdfd SD04G 3.69 GiB

mmcblk0: unknown partition table

eth0: Freescale FEC PHY driver Generic PHY (mii_bus:phy_addr=0:00, irq=-1)

标记 (2)
0 项奖励
回复
1 解答
2,890 次查看
shenjin
Contributor II

Hi jimmychan,

     we are using the version of 10.11. I will download the version of 11.09 for a test. later i will reply the testing results.
thanks!

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,890 次查看
shenjin
Contributor II

if we do a menuconfig about usb as bellow and make the otg ID pin to ground,we can find a mass storage device in the windows device manager,but if the otg ID pin floating,the kernel running stop on the above message all the same:

CONFIG_USB_EHCI_ARC_OTG—Enable support for the USB OTG port in HS/FS Host

mode.built as Y

•    CONFIG_USB_GADGET—USB Gadget Support: built as y

•    CONFIG_USB_OTG —OTG Support: built as Y

•    CONFIG_MXC_OTG—USB OTG pin detect support for UTMI PHY: built as Y

•    build USB GADGET driver as M, for example:

CONFIG_USB_ETH — usb ethernet gadget , build as M

CONFIG_USB_FILE_STORAGE—usb mass storage gadget, build as M

then , if you want to use EVK as mass storage device, insmod g_file_storage.ko

file=/dev/mmcblk0p2

why the otg ID pin can produce the effect?

0 项奖励
回复
2,890 次查看
jimmychan
NXP TechSupport
NXP TechSupport

which BSP are you using?

Please try the ver. 11.09 BSP. you can download it from the i.MX53QSB web page:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB

11.09 can also support iMX51. In fact, each freescale BSP release can support all iMX chip but we only do the fully test on one platform. For 11.09, we only done the fully test for iMX53. But from the ver 10.11 to 11.09, we had already fixed many USB related issues which can also be used on iMX51.

So please try the latest BSP first. If it works, you can update your BSP to Freescale new version or back porting the USB related driver from latest BSP to your BSP version.


2,891 次查看
shenjin
Contributor II

Hi jimmychan,

     we are using the version of 10.11. I will download the version of 11.09 for a test. later i will reply the testing results.
thanks!

0 项奖励
回复
2,890 次查看
shenjin
Contributor II

dear jimmychan,

      As you said,when we using the version of 11.09 ,the issue was solved and kernel can running well Although ID pin is also floating,the OTG function can doing as a host or a device According to the ID pin's states.

thank you very much.

0 项奖励
回复