imx35_sdio_timeout

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx35_sdio_timeout

1,565 Views
nancy
Contributor I

I am using imx35 board and wince 6 on that.

inserted sdio card and started to download one file from internet (around 100mb).while downloding the sdio driver gets timeout and not responding.Then only one way is rebooting the device.

the log file of sdio debugging is

Call NdisMQueryInformationComplete With FAILURE

GetCmdFromQueueToExecute()

command timeout (0x1f) ********

:HCR_HOST_INT_STATUS_REGISTER (0x0)*

HCR_HOST_INT_MASK_REGISTER (0x3)*

UPLOAD_HOST_INT_STATUS_RDY (0x1)*

[TT] INT NO upload status (int:0x0, mask:0x3)

MISC - Command TIME OUT !!

Call NdisMQueryInformationComplete With FAILURE

GetCmdFromQueueToExecute()

command timeout (0x6) ********

HCR_HOST_INT_STATUS_REGISTER (0x0)*

HCR_HOST_INT_MASK_REGISTER (0x3)*

UPLOAD_HOST_INT_STATUS_RDY (0x1)*

[TT] INT NO upload status (int:0x0, mask:0x3)

MISC - Command TIME OUT !!

what will be the problem?

0 Kudos
Reply
1 Reply

1,408 Views
karina_valencia
NXP Apps Support
NXP Apps Support

Deactivated user can you help on this case?

0 Kudos
Reply