imx35_sdio_timeout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx35_sdio_timeout

1,601件の閲覧回数
nancy
Contributor I

I am using imx35 board and wince 6 on that.

inserted sdio card and started to download one file from internet (around 100mb).while downloding the sdio driver gets timeout and not responding.Then only one way is rebooting the device.

the log file of sdio debugging is

Call NdisMQueryInformationComplete With FAILURE

GetCmdFromQueueToExecute()

command timeout (0x1f) ********

:HCR_HOST_INT_STATUS_REGISTER (0x0)*

HCR_HOST_INT_MASK_REGISTER (0x3)*

UPLOAD_HOST_INT_STATUS_RDY (0x1)*

[TT] INT NO upload status (int:0x0, mask:0x3)

MISC - Command TIME OUT !!

Call NdisMQueryInformationComplete With FAILURE

GetCmdFromQueueToExecute()

command timeout (0x6) ********

HCR_HOST_INT_STATUS_REGISTER (0x0)*

HCR_HOST_INT_MASK_REGISTER (0x3)*

UPLOAD_HOST_INT_STATUS_RDY (0x1)*

[TT] INT NO upload status (int:0x0, mask:0x3)

MISC - Command TIME OUT !!

what will be the problem?

0 件の賞賛
返信
1 返信

1,444件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

Deactivated user can you help on this case?

0 件の賞賛
返信