imx28 kernel time stamp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx28 kernel time stamp

1,446件の閲覧回数
shashikanthirem
Contributor III

Hi All.

i need to timer expiry calculation in micro sec, whose value is feed by user space using ioctl, but want to whats the best way to timestamp which is used in IRQ calls for example

serial_IRQ....{

// read byte for every byte

// get time stamp in usec ...???

}

1. this should take care of roll over

2. i am  using a do_gettimeofday() will it delay the irq ?

ラベル(2)
0 件の賞賛
返信
1 返信

1,378件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi shashikant

one can look at answers provided on

i.mx28 system timer/clock problem 

c - reading the timestamp from kernel using procfs - where is it stored after reading from kernel? -... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信