imx28 i2c timing issue with optimization flag

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx28 i2c timing issue with optimization flag

2,895 Views
shashikanthirem
Contributor III

Hi All,

I am using i2c send and receive written local i2c function call, which am seeing a I2C querry success and perfectly when I enable optimization(-O0) debug symbols, but does not works(NACK) when i remove the above (-O0)  compiler from the Makefie.

Any suggestion would be helpful

using 

linux 2.635.3, LTIB

Labels (2)
Tags (1)
0 Kudos
Reply
3 Replies

2,750 Views
shashikanthirem
Contributor III

pastedImage_1.png

pastedImage_2.png

0 Kudos
Reply

2,748 Views
igorpadykov
NXP Employee
NXP Employee

Hi shashikant

one can look at attached documentation about new ltib toolchain

and test if this helps.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,748 Views
shashikanthirem
Contributor III

i cannot do as of now.. 

0 Kudos
Reply