imx28 error boot nand

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx28 error boot nand

1,519件の閲覧回数
peterbärtsch
Contributor III

Hello

I try to boot from nand flash. But I get an error.

Output form console:

0x80508002

0x80508002

I made the bootsream with the mxsboot tool.

nand dump from barebox:

md -s /dev/nand0

00000000: 00000000 00000000 00000000 fffffcd6                ................

00000010: 20424346 01000000 06193c50 00000000                FCB ....P<......

00000020: 00000800 00000840 00000040 00000000                ....@...@.......

00000030: 00000000 00000000 00000004 00000200                ................

00000040: 00000200 00000004 0000000a 00000003                ................

00000050: 00000000 00000000 00000000 00000000                ................

00000060: 00000000 00000000 00000000 00000000                ................

00000070: 00000000 00000200 00000400 00000200                ................

00000080: 00000200 00000100 000007cf 00000000                ................

00000090: 00000800 00000000 00000000 00000000                ................

000000a0: 00000000 00000000 00000000 00000000                ................

000000b0: 00000000 00000000 00000000 00000000                ................

000000c0: 00000000 00000000 00000000 00000000                ................

000000d0: 00000000 00000000 00000000 00000000                ................

000000e0: 00000000 00000000 00000000 00000000                ................

000000f0: 00000000 00000000 00000000 00000000                ................


We use a S34MS01 1Gb Spansion flash on our board.

I try to set ROM4 NAND_ROW_ADDRESS_BYTES to 2. But without succsess.


I can't understand why the system doesn't boot.



Have anybody a idea?

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

1,200件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Peter

FSL does not support mxsboot, however one can try use

MFG Tool and link below

I.MX28_MFG_TOOL_LINUX : Tool and documentation for downloading i.MX28 image during manufacturing.

Re: NAND device unrecognized with an Update Error 0xffffffea(-22)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信