imx-atf boot flow

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,491件の閲覧回数
rkohli2000
Contributor III

Hi,

imx-atf allows alternative boot flow by preloading a BL33 (custom) image into memory.

Are there any instructions on how to use BL2 to boot an EL3 payload for pre-production test work ? Can we use EL3_PAYLOAD_BASE option ? Can someone point to some example instructions/app notes?

Also, there is the FIP build command "make PRELOADED_BL33_BASE=0x80000000 PLAT=imx8qm all fip". Does i.MX8QM plaform support this? Can it be used to allow booting a custom image (like Linux kernel or some app) from TF-A ?

Thanks for any suggestions.

0 件の賞賛
返信
1 解決策
4,429件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Yes, this is supported, but it has never implemented from our side

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
4,430件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Yes, this is supported, but it has never implemented from our side

 

0 件の賞賛
返信