iRAM area is not accessible with JTAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iRAM area is not accessible with JTAG

870 Views
admin
Specialist II

Saved FAQ from Freescale.com for information only:

Topic

JTAG

Debugger

 

Question.  The iRAM area(0x1FFE_0000) is not accessible with JTAG (RV-ICE).

 

Answer. 

1. Please check if ARM core of the i.MX51 is in supervisor mode, when using JTAG. Say, sometimes it may be in thumb one, since internal bootloader uses the thumb mode.

 

2. "Strange" behavior may be detected, if some i.MX51 fuses are "unexpectedly" burned because of power up sequence violation. Let me remind, VDD_FUSE is recommended be floated and grounded.

 

3.After watchdog reset internal memory IRAM is not accessible. Note, internal and UART / USB bootloader start watchdog.

 

 Related Products:

 i.MX Applications Processors > i.MX51 Processors > i.MX512, i.MX513, i.MX514, i.MX515, i.MX516

Tags (1)
0 Kudos
Reply
0 Replies