iMx6ull File-System Corruption issue on "rootfs" Partition during Bootup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMx6ull File-System Corruption issue on "rootfs" Partition during Bootup

1,467 次查看
niravagrawal
Contributor I

Hello Folks,

We are using iMx6ull based custom linux board with below BSP version.

Linux Kernal-Version = 4.19.35

DISTRO_VERSION = "4.19-warrior"

On one of the device, we are facing fs-corruption issue due to which processor could not recover by itself (kernel-panic!) and need some manual intervention to reset it and fix corrupted partition by running e2fs tools.

We have shared an issue log here. Please let us know if this issue has some genuine kernel bug (as it is related with low level JDB2 kthread) and any patch available or can be done to fix it.

This issue is seen on the device with long-run (2 to 4 months).  What we are suspecting is that why kernel thread is not recovering corrupted descriptor-block automatically ? (if checksum failed?)

Any help appreciated!

Regards,

Nirav Agrawal

 

 

 

 

 

0 项奖励
回复
1 回复

1,451 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nirav

 

for specific kernel ubifs issues may be recommended to post on dedicated linux forums

http://www.linux-mtd.infradead.org/faq/ubi.html

https://linux-mtd.infradead.narkive.com/2AmLFuhy/ubi-ubifs-problem

 

Best regards
igor

0 项奖励
回复