iMx6 WEC7 viedo decoding issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMx6 WEC7 viedo decoding issue

1,531件の閲覧回数
massimomilanesi
Contributor I

Hi,

working with WEC7 BSP v1.6 for iMx6 from Adeneo, I encountered a problem in trying to play a fullHD video:

using playwnd.exe I've tried to play from USB key the sample video:

http://mirrorblender.top-ix.org/peach/bigbuckbunny_movies/big_buck_bunny_1080p_h264.mov

the playing is not flowing mainly in the initial fase then tends to improve even if it has other jerky scenes.


The read speed from USB is about 15.5 MB/s, sufficient for the bitrate of the movie (about 10.000 kbps).

Using the other sample videos with lower resolution, present on:

http://mirrorblender.top-ix.org/peach/bigbuckbunny_movies/

the playing is correcly flowing, as if I encode again the FulHD movie with a lower bitrate (6.000 kbps and 4.000kbps).


Analyzing the real variable bitrate of 'big_buck_bunny_1080p_h264.mov', I've found that there are bitrate peaks in the points where the video runs bad (nearly 30.000kbps).

After this, I suppose that there are a sort of limitation/issue in video decoding library released with Adeneo BSP (in binary format).

Is this consideration correct?

Where can I find an updated revision of this library?

Note that the same board with Linux, works fine.


Thanks

Best regards,

Massimo



ラベル(5)
0 件の賞賛
返信
1 返信

1,378件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Deactivated user, Can you please comment on this issue?

0 件の賞賛
返信