iMXRT1172 SNVS bank -ON/OFF pin function query

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMXRT1172 SNVS bank -ON/OFF pin function query

Jump to solution
691 Views
vihang_vinayak
Contributor II

Hi,

We are using the iMXRT1172 in one of the battery application project. In my project to put iMXRT1172 in SNVS mode we are using the ONOFF pin (Ball no: U10) 

We just want to know if the ONOFF pin is independent of the execution code incase if the firmware gets stuck internally. I should be able to use the functionality of emergency off using the ONOFF pin.

Please confirm that the ONOFF pin is independent of the execution of code.

Quick response is appreciated.

Best Regards,

Vihang Waze

Design Engineer

Tata Elxsi Limited

0 Kudos
Reply
1 Solution
672 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Yes, the ONOFF pin is independent of the execution of code.

 

BR,

Edwin.

View solution in original post

0 Kudos
Reply
2 Replies
669 Views
vihang_vinayak
Contributor II

Thank you Edwin for the confirmation

0 Kudos
Reply
673 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Yes, the ONOFF pin is independent of the execution of code.

 

BR,

Edwin.

0 Kudos
Reply