iMX8qm Boot Core A72_0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8qm Boot Core A72_0

1,006 Views
kamohan
Contributor I

Hello NXP Forum,

on iMX8qm, can we have the bootup done from A72 core? Does SCUFW permit that.

Thanks

0 Kudos
Reply
8 Replies

603 Views
kamohan
Contributor I
Where can we get SCFW reference manual or design manual to make modification to SCFW firmware
0 Kudos
Reply

520 Views
kamohan
Contributor I
How do we get our own customised logs in SCFW?

Thanks
Mohan
0 Kudos
Reply

592 Views
yipingwang
NXP TechSupport
NXP TechSupport

You can start here:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101/ta-p/1124...

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Getting-s...

 

The SCFW reference/porting documentation is supplied inside the NXP SCFW Porting Kit , rather than as a separate public reference manual.

  • Download the kit from the NXP i.MX Software and Development page. Select the release corresponding to your i.MX BSP; NXP requires the matching porting kit to maintain compatibility with its supplied binaries.
  • Accept the license and run the included .bin installer.
  • Look under:
    • doc/pdf/sc_fw_port.pdf — detailed SCFW Porting Guide
    • doc/pdf/ — SCFW API User Guide, release notes, and related documentation
    • src/ — SoC-specific SCFW export archives

The kit contains a mixture of source and object code. Board-dependent customization is performed in the exported board sources—typically under platform/board/mx8<device>_<board>/ , including files such as board.c ; much of the core SCFW remains object-only and cannot be modified through the public kit.

The general i.MX Porting Guide, UG10165 , also has a “Porting System Controller Firmware” chapter and explains integration with the BSP and meta-imx-scfw.

0 Kudos
Reply

945 Views
kamohan
Contributor I

Hello,

I have followed the following steps to build bootloader, but the bootloader fails without any logs.

Could you please validate attached steps.

Thanks

 

mkdir Scarthgap_New
cd Scarthgap_New
 
1. Get the Security Controller Binaries
mkdir SECO
cd SECO
chmod +x imx-seco-5.9.4.1-0333596.bin
./imx-seco-5.9.4.1-0333596.bin
 
mkashyap@cse-dev02:~/iMX8/Scarthgap_New/SECO/imx-seco-5.9.4.1-0333596/firmware/seco$ ls -al
total 976
drwxrwxr-x 2 mkashyap mkashyap   4096 Aug 26 22:21 .
drwxrwxr-x 3 mkashyap mkashyap   4096 Aug 26 22:21 ..
-rw-r--r-- 1 mkashyap mkashyap    194 Jul 29  2024 commit-id.txt
-rw-r--r-- 1 mkashyap mkashyap 163840 Jul 29  2024 mx8dxla1-ahab-container.img
-rw-r--r-- 1 mkashyap mkashyap 163840 Jul 29  2024 mx8dxlb0-ahab-container.img
-rw-r--r-- 1 mkashyap mkashyap  76944 Jul 29  2024 mx8qmb0-ahab-container.img
-rw-r--r-- 1 mkashyap mkashyap  71312 Jul 29  2024 mx8qxb0-ahab-container.img
-rw-r--r-- 1 mkashyap mkashyap  78408 Jul 29  2024 mx8qxc0-ahab-container.img
-rwxr-xr-x 1 mkashyap mkashyap 423875 Jul 29  2024 SECO_FW_release_note.pdf
mkashyap@cse-dev02:~/iMX8/Scarthgap_New/SECO/imx-seco-5.9.4.1-0333596/firmware/seco$
 
we use mx8qmb0-ahab-container.img
 
cd ../../../..
 
2. Download and build ATF
mkdir ATF
cd ATF
git clone https://github.com/varigit/imx-atf -b lf_v2.10_6.6.52-2.2.0_var01
 
cd imx-atf
source /opt/fsl-imx-xwayland/6.6-scarthgap/environment-setup-armv8a-poky-linux
unset LDFLAGS
make PLAT=imx8qm bl31
 
mkashyap@cse-dev02:~/iMX8/Scarthgap_New/ATF/imx-atf/build/imx8qm/release$ ls -al
total 76
drwxrwxr-x 7 mkashyap mkashyap  4096 Aug 26 22:37 .
drwxrwxr-x 3 mkashyap mkashyap  4096 Aug 26 22:36 ..
drwxrwxr-x 3 mkashyap mkashyap  4096 Aug 26 22:37 bl31
-rwxrwxr-x 1 mkashyap mkashyap 45213 Aug 26 22:37 bl31.bin
drwxrwxr-x 2 mkashyap mkashyap  4096 Aug 26 22:37 lib
drwxrwxr-x 2 mkashyap mkashyap  4096 Aug 26 22:37 libc
drwxrwxr-x 2 mkashyap mkashyap  4096 Aug 26 22:37 libwrapper
drwxrwxr-x 2 mkashyap mkashyap  4096 Aug 26 22:37 romlib
 
cd ../../../../../
 
3. Download and build SCFW
   mkdir SCFW
   cd SCFW
   
   sudo tar xf gcc-arm-none-eabi-8-2018-q4-major-linux.tar.bz -C ./opt
   
   cd imx-sc-firmware/src/scfw_export_mx8qm_b0
   
   export TOOLS=/home/mkashyap/iMX8/Scarthgap_New/SCFW/Opt
   make clean-qm
   make qm R=B0 B=var_som V=1
   
   mkashyap@cse-dev02:~/iMX8/Scarthgap_New/SCFW/imx-sc-firmware/src/scfw_export_mx8qm_b0/build_mx8qm_b0$ ls -al
   total 3384
   drwxrwxr-x 11 mkashyap mkashyap    4096 Aug 26 22:47 .
   drwxrwxr-x  6 mkashyap mkashyap    4096 Aug 26 22:47 ..
   drwxrwxr-x  3 mkashyap mkashyap    4096 Aug 26 22:47 board
   drwxrwxr-x  3 mkashyap mkashyap    4096 Aug 26 22:44 devices
   drwxrwxr-x 25 mkashyap mkashyap    4096 Aug 26 22:47 drivers
   drwxrwxr-x  2 mkashyap mkashyap    4096 Aug 26 22:44 main
   -rwxrwxr-x  1 mkashyap mkashyap  184448 Aug 26 22:47 scfw_tcm.bin
   -rwxrwxr-x  1 mkashyap mkashyap 2787784 Aug 26 22:47 scfw_tcm.elf
   -rw-rw-r--  1 mkashyap mkashyap  513123 Aug 26 22:47 scfw_tcm.map
   drwxrwxr-x  4 mkashyap mkashyap    4096 Aug 26 22:44 soc
   drwxrwxr-x 26 mkashyap mkashyap    4096 Aug 26 22:44 ss
   drwxrwxr-x  9 mkashyap mkashyap    4096 Aug 26 22:47 svc
   drwxrwxr-x 10 mkashyap mkashyap    4096 Aug 26 22:44 test
   drwxrwxr-x  2 mkashyap mkashyap    4096 Aug 26 22:44 utilities
   
   cd ../../../../../
   
4. Build u-boot
   mkdir u-boot
   cd u-boot
   
   git clone https://github.com/varigit/uboot-imx.git -b lf_v2024.04_6.6.52-2.2.0_var01
   cd uboot-imx
   
   cp ../../SECO/imx-seco-5.9.4.1-0333596/firmware/seco/mx8qmb0-ahab-container.img ./mx8qm-ahab-container.img
   cp ../../SCFW/imx-sc-firmware/src/scfw_export_mx8qm_b0/build_mx8qm_b0/scfw_tcm.bin ./mx8qm-mek-scfw-tcm.bin
   make mrproper
   make imx8qm_var_som_defconfig
   make -j8
   
   cd ../../
   
5. Make Image 
   mkdir MkImage
   cd MkImage
   
   git clone https://github.com/varigit/imx-mkimage -b lf-6.6.52_2.2.0_var01
   cd imx-mkimage
   
   cp ../../SECO/imx-seco-5.9.4.1-0333596/firmware/seco/mx8qmb0-ahab-container.img ./iMX8QM/
   cp ../../SCFW/imx-sc-firmware/src/scfw_export_mx8qm_b0/build_mx8qm_b0/scfw_tcm.bin ./iMX8QM/
   cp ../../u-boot/uboot-imx/u-boot.bin ./iMX8QM/
   cp ../../u-boot/uboot-imx/spl/u-boot-spl.bin ./iMX8QM/
   cp ../../ATF/imx-atf/build/imx8qm/release/bl31.bin ./iMX8QM/
   
   make SOC=iMX8QM flash_ca72
   
   cd iMX8QM
   make -f soc.mak SOC=iMX8QM MKIMG=../mkimage_imx8 PAD_IMAGE=./pad_image.sh flash_ca72
   
   mkashyap@cse-dev02:~/iMX8/Scarthgap_New/MkImage/imx-mkimage/iMX8QM$ ls -al
   total 6792
   drwxrwxr-x  3 mkashyap mkashyap    4096 Aug 26 23:08 .
   drwxrwxr-x 13 mkashyap mkashyap    4096 Aug 26 23:06 ..
   -rwxrwxr-x  1 mkashyap mkashyap   45213 Aug 26 23:06 bl31.bin
   -rwxrwxr-x  1 mkashyap mkashyap    2564 Aug 26 22:59 expand_c_define.sh
   -rw-rw-r--  1 mkashyap mkashyap 1895424 Aug 26 23:08 flash.bin
   -rw-rw-r--  1 mkashyap mkashyap       9 Aug 26 23:06 head.hash
   -rwxrwxr-x  1 mkashyap mkashyap    2078 Aug 26 22:59 mkimage_fit_atf.sh
   -rw-r--r--  1 mkashyap mkashyap   76944 Aug 26 23:02 mx8qmb0-ahab-container.img
   -rwxrwxr-x  1 mkashyap mkashyap  184448 Aug 26 23:03 scfw_tcm.bin
   drwxrwxr-x  2 mkashyap mkashyap    4096 Aug 26 22:59 scripts
   -rwxrwxr-x  1 mkashyap mkashyap   13271 Aug 26 22:59 soc.mak
   -rwxrwxr-x  1 mkashyap mkashyap 1631521 Aug 26 23:06 u-boot-atf.bin
   -rw-rw-r--  1 mkashyap mkashyap 1500440 Aug 26 23:04 u-boot.bin
   -rw-rw-r--  1 mkashyap mkashyap 1500449 Aug 26 23:06 u-boot-hash.bin
   -rw-rw-r--  1 mkashyap mkashyap  139387 Aug 26 23:04 u-boot-spl.bin
 
 
The generated flash.bin was used as an bootloader image

 

0 Kudos
Reply

939 Views
yipingwang
NXP TechSupport
NXP TechSupport

For your specific procedure, the important point is this:

make SOC=iMX8QM flash_ca72

is the correct target conceptually if your intent is to load the bootloader to the A72 instead of the A53 . NXP community guidance describes flash_ca72 as similar to the basic flash_b0 image, but loaded to the A72 rather than the A53 .

The “no logs” symptom does not automatically mean SCFW rejected A72 boot . A known gotcha is that A53 and A72 do not use the same log terminal , so if you monitor the usual A-core/A53 UART you may see nothing even though the A72 image is running or failing later on a different console path.

Validation of your steps:

Area

Assessment

SECO container

mx8qmb0-ahab-container.img is the right class of container for i.MX8QM B0.

ATF

make PLAT=imx8qm bl31 is reasonable for i.MX8QM.

SCFW

Building make qm R=B0 B=var_som V=1 is consistent with an i.MX8QM B0 Variscite target.

U-Boot

imx8qm_var_som_defconfig is the key item to confirm: it must be compatible with the A72 boot path and console configuration.

mkimage target

flash_ca72 is the right target only for A72 boot. For normal Linux BSP boot, the documented i.MX8QM command is make SOC=iMX8QM flash .

SPL copy

u-boot-spl.bin is likely irrelevant for flash_ca72 ; that target is not the SPL-based flow.

Duplicate image build

Running both top-level make SOC=iMX8QM flash_ca72 and then manually running make -f soc.mak ... flash_ca72 is unnecessary. Use one clean top-level command.

I would correct/clean the image-generation part to:

cd ~/iMX8/Scarthgap_New/MkImage/imx-mkimage

 

cp ../../SECO/imx-seco-5.9.4.1-0333596/firmware/seco/mx8qmb0-ahab-container.img ./iMX8QM/

cp ../../SCFW/imx-sc-firmware/src/scfw_export_mx8qm_b0/build_mx8qm_b0/scfw_tcm.bin ./iMX8QM/

cp ../../u-boot/uboot-imx/u-boot.bin ./iMX8QM/

cp ../../ATF/imx-atf/build/imx8qm/release/bl31.bin ./iMX8QM/

 

make clean

make SOC=iMX8QM flash_ca72

Then use:

iMX8QM/flash.bin

Also fix/check this SCFW path:

export TOOLS=/home/mkashyap/iMX8/Scarthgap_New/SCFW/Opt

You extracted into ./opt , but exported .../SCFW/Opt . Linux paths are case-sensitive. Since you did produce scfw_tcm.bin , your actual shell may have had a valid tool path, but this line should be verified.

Recommended debug sequence:

  • First build and boot the standard image:

make SOC=iMX8QM flash

This checks that SECO + SCFW + ATF + U-Boot + board DDR/console are basically correct. The Linux User’s Guide documents this standard i.MX8QM flash.bin generation path.

  • Then rebuild with:

make SOC=iMX8QM flash_ca72

  • Monitor the A72 console/UART , not only the normal A53 console. The A53 and A72 log terminals differ.
  • If still silent, compare the generated flash.bin size/layout between flash and flash_ca72 , and confirm that the Variscite U-Boot config actually enables the console used by the A72 boot target.

So the direct answer is: SCFW does permit starting the Cortex-A side on A72 through the flash_ca72 image flow, but SCFW still owns the initial boot orchestration. Your procedure is mostly valid for A72 boot, but remove the duplicate soc.mak invocation, verify the SCFW tool path, and most importantly check the A72 UART/console.

Takeaway: A72 boot on i.MX8QM is supported via flash_ca72 ; a silent boot is more likely an image/config/console issue than SCFW simply refusing to start A72.

 

0 Kudos
Reply

980 Views
yipingwang
NXP TechSupport
NXP TechSupport

Yes — on i.MX8QM, the application-processor boot image can be targeted to the Cortex-A72 instead of the Cortex-A53, and SCFW permits that flow. NXP’s imx-mkimage has a flash_ca72 target described as the A72 variant of the normal A53 boot image, intended to bring up the A72 as early as possible for boot-time optimization .

The important distinction is:

  • First code after reset: not the A72. The device boot flow still starts through ROM/SCU/SCFW.
  • AP-side bootloader / OS bring-up: yes, this can be done on the A72. SCFW initializes DDR, loads Cortex-A images, then boots the cores and sets their start addresses.
  • Configuration mechanism: the boot container can specify an AP image for a72 , e.g. examples show -ap ... a72 ... in imx-mkimage usage.

So the answer is: SCFW does allow booting the AP software path from A72, but A72 is not the reset/ROM boot master; it is started by SCFW according to the boot container configuration.

0 Kudos
Reply

973 Views
kamohan
Contributor I
There is a small point we would like to clarify/validate: the `flash_ca72` target currently references `u-boot-atf.bin`, while a separate `u-boot-atf-a72.bin` is also available in the same configuration.

How do we proceed
0 Kudos
Reply

970 Views
yipingwang
NXP TechSupport
NXP TechSupport

Proceed with the existing flash_ca72 target first; do not replace u-boot-atf.bin with u-boot-atf-a72.bin unless you are intentionally using the cockpit / multi-AP image flow.

The evidence points to this distinction:

  • flash_ca72 is described as the same basic boot image as the normal A-core boot target, but loaded to the A72 instead of the A53.
  • u-boot-atf.bin is the combined ATF + U-Boot image: bl31.bin plus u-boot.bin / u-boot-hash.bin .
  • u-boot-atf-a72.bin appears in the flash_cockpit target, where the image contains two AP payloads : one for A53 and a separate one for A72: -ap u-boot-atf.bin a53 0x80000000 ... -ap u-boot-atf-a72.bin a72 0xC0000000 ... .

So the important selector is not only the filename; it is the imx-mkimage -ap ... a72 ... argument in the target. For a single A72 boot image, flash_ca72 using u-boot-atf.bin is consistent with the documented intent: the payload is loaded to A72 by the target rule, even if the filename is not suffixed -a72 .

Recommended path:

  • Build the standard A72-only image using the existing target:

make SOC=iMX8QM flash_ca72

  • Use the CA72 device tree / configuration on the Linux side. NXP documentation notes that the i.MX8QM MEK CA72 DTB supports the two Cortex-A72 cores only and requires the special boot image built with flash_ca72 .
  • Reserve u-boot-atf-a72.bin for flows that explicitly package a second A72 AP image, such as flash_cockpit , unless your BSP’s soc.mak comments or release notes say otherwise.
  • Validate at boot that the image is actually entering the A72 path: check the imx-mkimage command emitted by make V=1 SOC=iMX8QM flash_ca72 or inspect iMX8QM/soc.mak and confirm the AP line uses a72 .

Takeaway: treat the current flash_ca72 reference to u-boot-atf.bin as intentional; u-boot-atf-a72.bin is for the separate A72 payload used in cockpit/multi-partition style images, not automatically the replacement for flash_ca72 .

 

0 Kudos
Reply