iMX8Quad Gstreamer Interpipe support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8Quad Gstreamer Interpipe support

3,360件の閲覧回数
ottob
Contributor IV

Hi There !

The project I am working in requires dynamic pipelines, like what is shown here - https://developer.ridgerun.com/wiki/index.php?title=NVIDIA_GTC_2020:_How_to_build_a_multi-camera_Med...

 

So far I have not had any luck getting this working for the iMX8QuadMax. As a test I created this pipeline - 

gst-launch-1.0 filesrc location=/run/media/sda1/h264_test_stream.ts ! video/mpegts ! tsdemux ! queue ! h264parse ! v4l2h264dec ! interpipesink name=camera0 forward-events=true forward-eos=true sync=false interpipesrc listen-to=camera0 ! imxvideoconvert_g2d ! waylandsink

Which returns an error - gst_inter_pipe_sink_get_caps:<camera0> Failed to obtain an intersection between upstream elements and listeners. I also tried modifying the GTC2020 media server example, see attached. That results in a cap error 

 

** (gstd:1913): CRITICAL **: 00:30:20.490: gst_video_info_from_caps: assertion 'caps != NULL' failed
0:00:09.788343495 1913 0xffffa813a370 WARN waylandsink wlvideoformat.c:145:gst_video_format_to_wl_dmabuf_format: wayland dmabuf video format not found
0:00:09.788443995 1913 0xffffa813a370 WARN videopool gstvideopool.c:215:video_buffer_pool_set_config:<waylandpool0> no caps in config

 

Looks like the waylandsink is having trouble reading the caps through the interpipe

 

Has anyone had any luck doing this ? If its currently not supported in the NXP gstreamer plugins, is that something we can pay (NXP) to have implemented ? 

Thanks in advance,

/Otto 

 

 

0 件の賞賛
返信
1 返信

3,339件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi @ottob,

 

Yes, is something you can paid to our professional service that are available on the next link, the cost depends on the application, but they can give you a better approach:

[email protected]
[email protected]
https://www.nxp.com/support/support/nxp-engineering-services/professional-engineering-services:PROFE...
https://www.nxp.com/support/support/nxp-engineering-services/professional-support-for-processors-and...

 

Regards,

Israel.