Is it possible to populate an iMX8QXP based board with different RAM sizes (8Gb, 16Gb, 24Gb, 32Gb) and handle this with the same scfw/u-boot/kernel image? Different RAM sizes would be configured in user fuses. scfw should then dynamically adjust the RAM size according to the fuse settings. Is there an example for such an approach?
解決済! 解決策の投稿を見る。
Hello,
No this is not possible, please note that ROM code will read and execute the SCFW, this will include the DDR initialization. Also, we do not have such approach.
Best regards,
Aldo.
Hello,
No this is not possible, please note that ROM code will read and execute the SCFW, this will include the DDR initialization. Also, we do not have such approach.
Best regards,
Aldo.