iMX8QM end Kernel panic

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8QM end Kernel panic

4,176件の閲覧回数
Ray_chentao
Contributor I

 

hello,

I am having a kernel panic problem with the processor  iMX8QM. The DDR Stress Test is OK, what can I do to debug this problem, the error log is attached.

CPU: Freescale i.MX8QM revB A53 at 1200 MHz at 55C
Model: Freescale i.MX8QM MEK
Board: iMX8QM MEK
Boot: MMC0
DRAM: 6 GiB

 

[ 2.538851] [<ffff000008083230>] el1_irq+0xb0/0x124
[ 2.546978] imx8-dpr-channel 570f0000.dpr-channel: Linked as a consumer to 57060000.prg
[ 2.554505] [<ffff000008085820>] arch_cpu_idle+0x10/0x18
[ 2.554508] [<ffff00000810d8a0>] do_idle+0x120/0x1e0
[ 2.554511] [<ffff00000810dafc>] cpu_startup_entry+0x24/0x28
[ 2.554518] [<ffff00000808fac8>] secondary_start_kernel+0x110/0x120
[ 2.564677] imx8-dpr-channel 57100000.dpr-channel: Linked as a consumer to 57070000.prg
[ 2.570352] Code: bad PC value
[ 2.570365] ---[ end trace bcd121847d8b8700 ]---
[ 2.578229] imx8-dpr-channel 57100000.dpr-channel: Linked as a consumer to 57080000.prg
[ 2.586022] Kernel panic - not syncing: Fatal exception in interrupt
[ 2.586026] SMP: stopping secondary CPUs
[ 2.593865] Kernel Offset: disabled
[ 2.593868] CPU features: 0x180200d
[ 2.593869] Memory Limit: none
[ 2.882678] ---[ end Kernel panic - not syncing: Fatal exception in interrupt

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,963件の閲覧回数
achintala
Contributor I

How was this issue solved? @Ray_chentao - I'm running into same problem, would be great to learn from your experience on solving this.

0 件の賞賛
返信

4,164件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @Ray_chentao 

You should check your DDR Calibration again.

0 件の賞賛
返信

4,149件の閲覧回数
Ray_chentao
Contributor I

Hi, @Qmiller, thanks a lot.

How could I check my DDR Calibration?  Use i.MX8 DDR Tools and run the DDR stress test?

The DDR stress test is succeed at DDR clock 800MHz and 1200MHz, but  fail at 1600MHz.

We're trying to config my iMX8QM work at DDR clock 800MHz, but the problem was still occurred with the same log.

 

 

0 件の賞賛
返信