iMX8QM FUSB302 Type-C Initialization Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8QM FUSB302 Type-C Initialization Issue

1,849件の閲覧回数
prashanthkumar
Contributor II

Hi,

We are working on iMX8QM custom board with 4.14.78 Kernel BSP release, in which we are using "FUSB302" Kernel driver for USB 3.0 Type-C detection.

The USB Type-C devices detecting as 3.0 (Super Speed) during the hot plug, but during kernel boot the same is detecting as 2.0 (High Speed).

Detection during boot time:
usb 1-1: new high-speed USB device number 2 using cdns-usb3

Detection during hot plug:
usb 1-1: new SuperSpeed USB device number 2 using cdns-usb3


Is the same issue observed in iMX8QM reference board?
Kindly suggest the solution as soon as possible.

Best Regards,

Prashanth Kumar K

0 件の賞賛
返信
1 返信

1,662件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we are not able to assist you, since the i.MX8QM is still on preproduction and we do not have a way to test your problem. I apologize for the inconveniences this could give you.

Best regards,

Diego.

0 件の賞賛
返信