iMX8QM FUSB302 Type-C Initialization Issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX8QM FUSB302 Type-C Initialization Issue

1,852 次查看
prashanthkumar
Contributor II

Hi,

We are working on iMX8QM custom board with 4.14.78 Kernel BSP release, in which we are using "FUSB302" Kernel driver for USB 3.0 Type-C detection.

The USB Type-C devices detecting as 3.0 (Super Speed) during the hot plug, but during kernel boot the same is detecting as 2.0 (High Speed).

Detection during boot time:
usb 1-1: new high-speed USB device number 2 using cdns-usb3

Detection during hot plug:
usb 1-1: new SuperSpeed USB device number 2 using cdns-usb3


Is the same issue observed in iMX8QM reference board?
Kindly suggest the solution as soon as possible.

Best Regards,

Prashanth Kumar K

0 项奖励
回复
1 回复

1,665 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we are not able to assist you, since the i.MX8QM is still on preproduction and we do not have a way to test your problem. I apologize for the inconveniences this could give you.

Best regards,

Diego.

0 项奖励
回复