Hi Community,
I'm working with iMX8QM, u-boot 2020.04-imx_v2020.04_5.4.47_2.2.0. I'm trying to configure the RGMII 100Mbps Ethernet. PHY is Marvell 88q2110.
The ethernet reference clock should be :
- 25MHz when using 100Mbps Ethernet
- 125MHz when using 1Gbps Ethernet
From the datasheet below the RGMII operates at 125MHz.
Ingrid_0-1648731162475.png
Since I'm using 100Mbps ethernet I would like to use 25Mhz as the ethernet reference clock.
Currently when pinging the board from my computer, the activity led blinks on the iMX8 board but I get no response.
Here are my questions:
1 - Does the reference clock automatically switch when 100Mbps of 1Gbps is detected?
1a - If yes, is it connecting 25MHz on RGMII_TXC using CONN_ENET0_REFCLK_125M_25M?
Ingrid_1-1648731919930.png
1b - If not, how can I configure RGMII_TXC to use 25MHz?
At the moment I'm unable to check the clock due to the board being in a box but I will be able to scope that next week.
Here is what I have configured in my .dts
&fec1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_fec1>;
phy-mode = "rgmii-rxid";
phy-handle = <ðphy0>;
fsl,magic-packet;
fsl,rgmii_txc_dly;
status = "okay";
local-mac-address = [00 a8 44 1f 1f 10];
mdio {
#address-cells = <1>;
#size-cells = <0>;
ethphy0: ethernet-phy@4 {
compatible = "ethernet-phy-id002b.0980", "ethernet-phy-ieee802.3-c45";
reg = <4>;
max-speed = <100>;
};
};
};
pinctrl_fec1: fec1grp {
fsl,pins = <
SC_P_COMP_CTL_GPIO_1V8_3V3_ENET_ENETB_PAD 0x000014a0
SC_P_ENET0_MDC_CONN_ENET0_MDC 0x06000020
SC_P_ENET0_MDIO_CONN_ENET0_MDIO 0x06000020
SC_P_ENET0_RGMII_TXC_CONN_ENET0_RGMII_TXC 0x00000061
SC_P_ENET0_RGMII_TX_CTL_CONN_ENET0_RGMII_TX_CTL 0x00000061
SC_P_ENET0_RGMII_TXD0_CONN_ENET0_RGMII_TXD0 0x00000061
SC_P_ENET0_RGMII_TXD1_CONN_ENET0_RGMII_TXD1 0x00000061
SC_P_ENET0_RGMII_TXD2_CONN_ENET0_RGMII_TXD2 0x00000061
SC_P_ENET0_RGMII_TXD3_CONN_ENET0_RGMII_TXD3 0x00000061
SC_P_ENET0_RGMII_RXC_CONN_ENET0_RGMII_RXC 0x00000061
SC_P_ENET0_RGMII_RX_CTL_CONN_ENET0_RGMII_RX_CTL 0x00000061
SC_P_ENET0_RGMII_RXD0_CONN_ENET0_RGMII_RXD0 0x00000061
SC_P_ENET0_RGMII_RXD1_CONN_ENET0_RGMII_RXD1 0x00000061
SC_P_ENET0_RGMII_RXD2_CONN_ENET0_RGMII_RXD2 0x00000021
SC_P_ENET0_RGMII_RXD3_CONN_ENET0_RGMII_RXD3 0x00000061
>;
};
I also tried forcing the 25MHz by adding the following in the fec1 node
assigned-clocks = <&clk IMX8QM_ENET0_ROOT_DIV>, <&clk IMX8QM_ENET0_REF_DIV>;
assigned-clock-rates = <25000000>, <25000000>;
When I check clk dump I have the following. Also not sure why ENET0_RGMII_DIV is 0
Ingrid_2-1648734049288.png
Thanks for your help
Best Regards,
Ingrid