Hello,
I am developing on a custom board with iMX8QM on it.
I compiled the Android Automotive OS 12.0.0 image and ran it on the iMX8QM EVK board.
But the same image doesn't work on my custom board.
I found that the problem was caused by the "scfw-tcm.bin" binary.
I have a "scfw-tcm.bin" file that runs my Yocto image but I don't know from which source code it was generated.
I included the binary that runs my Yocto image in my Android Automotive OS BSP and recompiled.
After this process, I tried to upload my image, which I compiled with the "uuu_imx_android_flash.bat" script, to my custom board, but the installation cannot load the "u-boot-imx8qm-mek-uuu.imx" file and proceed to the next installation step.
When this upload is done in the Serial Port, I see a U-Boot flow, but then there is no intelligence and the upload stays here.
What changes can I make to the source file "${MY_ANDROID}/vendor/nxp/fsl-proprietary/uboot-firmware/imx8qm/board-imx8qm.c", which generates the "scfw-tcm.bin" file for this problem?
With what change in this source file can I get my image to run on my custom board?
Could you please help me with this issues?
Best regards,
Efecan
已解决! 转到解答。
Hi @Zhiming_Liu,
Thank you for your support and feedback.
I will review the document you referenced.
Best regards,
Efecan
Hi @cbl
If you have any dts change/ hardware reassign compared with MEK, you need follow below link to change and generate new SCFW firmware.
Regards
Zhiming