iMX8QM A0 CPU Soft Reset Issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX8QM A0 CPU Soft Reset Issue

2,057 次查看
prashanthkumar
Contributor II

Hi,

We are working on iMX8QM custom board with 4.14.98 Kernel BSP release with 'imx-scfw-porting-kit-1.2' SCFW.
The iMX8QM B0 CPU is able to do soft reset (reset command in u-boot & reboot command in kernel) , but the same soft reset is hanging for A0 CPU.

But  in iMX8QM A0 CPU able to do soft reset If we use 4.14.78 BSP with 'imx-scfw-porting-kit-1.1.2' SCFW source code.

Is there any CPU restriction/bug for iMX8QM A0 CPU soft reset in imx-scfw-porting-kit-1.2 SCFW or 4.14.98 Kernel BSP release? How to resolve this soft reset issue for A0 CPU?

Best Regards,

Prashanth Kumar K

0 项奖励
回复
1 回复

1,765 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Prashanth

L4.14.98 scfw changes are described in Chapter 2 

Change List System Controller Firmware Release Notes included in

SCFW Porting Kit

In general old revision A0 CPU is not supported in new BSPs.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复