iMX8MQ processor Socket Based EVK for secure boot (OTP)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8MQ processor Socket Based EVK for secure boot (OTP)

2,757件の閲覧回数
nilesh_patel
Contributor II

Hi,

We are planning to work for a secure Boot on iMX8MQ.

For secure boot, we need to program the fuses on i.MX8MQ(processor) and as per our understanding this is a one-time programmable process.

So in the development phase, we would require process steps where
1) A method by which we can reverse the false written fuses? As per our understanding this is not possible. Kindly confirm.
2) An EVK which contains the socket-based processor, whose processor chipset can be replaced. Request to provide the reference where such EVK with processor socket for our development.

Thanks,

Nilesh Patel

ラベル(2)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

2,662件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nilesh

1. yes this understanding is correct.

2. EVK board design files have bom file which lists all used parts.

i.MX 8M Evaluation Kit | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,662件の閲覧回数
nilesh_patel
Contributor II

Hi igor,

Is there any method, to avoid processor damage?

Thanks,

Nilesh Patel

0 件の賞賛
返信

2,662件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nilesh

 

>Is there any method, to avoid processor damage?

I am afraid no, as blown fuses can not be reverted back.

 

Best regards
igor

0 件の賞賛
返信