iMX8MQ RTC supply

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8MQ RTC supply

1,721件の閲覧回数
ani10c89
Contributor II

Hi,

For RTC back-up supply, so we need to provide both VDD_SNVS and NVCC_SNVS through external coin cell or supercap if RTC timings need to be stored? 

Please confirm.

Regards,

Anirudha

ラベル(1)
0 件の賞賛
返信
1 返信

1,595件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  You are right.  

According to section 3.1.6 (Power modes) of i.MX 8M  Data Sheet for Consumer Products,

Rev. 1.1, 07/2019 :

SNVS Mode: This mode is also called RTC mode. Only the power for the SNVS domain remains
on to keep RTC and SNVS logic alive.

  Table 10 (Chip power in different LP mode) states about VDD_SNVS and NVCC_SNVS

supply voltages for this mode.

https://www.nxp.com/docs/en/data-sheet/IMX8MDQLQCEC.pdf 


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 件の賞賛
返信