iMX8MPlus I2S Compatibility

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8MPlus I2S Compatibility

ソリューションへジャンプ
4,247件の閲覧回数
GuiDas
Contributor II

Hello,

I am developing a board with iMX8MPlus processor. I would like to use an audio Codec, TVL320AIC3007, but I have problem with the audio interface between the processor and the Codec.

Here is the interface of the Codec :

GuiDas_0-1624604219575.png

 

For the DIN and DOUT there is no problem as I can use the TX RX data of a SAI. For the clock I am more confused as I need two bidirectionnal clockand the SAI of the processor as only one of them.

 

My question is, is it possible to connect the Audio Codec to the processor ? If yes which SAI pins can be used for the BCLK and WCLK ?

 

Thank you in advance,

 

Guilhem

 

0 件の賞賛
返信
1 解決策
4,239件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Guilhem

 

from TLV320AIC datasheet:

BCLK - Audio serial data bus bit clock input/output

WCLK-Audio serial data bus word clock input/output

BCLK can be connected to SAI BCLK, direction is configured by "BCD" -

Bit Clock Direction described in sect.14.4

i.MX 8M Plus Applications Processor Reference Manual

WCLK is connected to SAI "Frame Sync" described in sect.14.4.3 External signals

direction is configured by "FSD"..

 

Best regards
igor

元の投稿で解決策を見る

2 返答(返信)
4,240件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Guilhem

 

from TLV320AIC datasheet:

BCLK - Audio serial data bus bit clock input/output

WCLK-Audio serial data bus word clock input/output

BCLK can be connected to SAI BCLK, direction is configured by "BCD" -

Bit Clock Direction described in sect.14.4

i.MX 8M Plus Applications Processor Reference Manual

WCLK is connected to SAI "Frame Sync" described in sect.14.4.3 External signals

direction is configured by "FSD"..

 

Best regards
igor

4,027件の閲覧回数
shifman
Contributor I

The IMX8MP have two SYNC signals, for example in SAI3 it have SAI3_RXFS and SAI3_TXFS.

in case we have an audio codec with one bidirectional LRCLK port, to which one of the two signals it should be connected to? SAI3_RXFS or SAI3_TXFS

Thank you

0 件の賞賛
返信