iMX8MM MIPI-CSI Controls

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8MM MIPI-CSI Controls

2,367件の閲覧回数
raajeshk88
Contributor III

Hi,

   I am using iMX8MM EVK along with MIPI-CSI board which comes with ov5640 camera sensor. The interface is working fine with image capture/streaming. But I need controls to achieve hflip,contrast/brightness adjustment. The driver is not instantiating a subdev which provides these controls. I tried to use ov5640_mipi_v3 driver to get the subdev driver but still could not get it. I am using the prebuilt images from 4.19.35. Kindly could provide information on achieving these controls (with or without subdev/v4l2). Thanks

0 件の賞賛
返信
2 返答(返信)

2,258件の閲覧回数
art
NXP Employee
NXP Employee

Please check the community thread below:

https://community.nxp.com/thread/524572

Hope it would be of some help.

Best Regards,
Artur

0 件の賞賛
返信

2,258件の閲覧回数
raajeshk88
Contributor III

Hi Artur,

           Thanks let me follow the thread and will update you on the outcome.

Regards,

Raajesh K

0 件の賞賛
返信