iMX8MM CSI2 ADV7282M Cannot capture

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8MM CSI2 ADV7282M Cannot capture

2,222件の閲覧回数
kbch
Contributor I

Hi

 

I'm trying to use the ADV7282M Video decoder with a iMX8MM Board and the Mainline ADV7180 Driver. I've added CONFIG_VIDEO_ADV7180=m to my Kernel config.

 

My device tree looks like this

 

 

&i2c2 {
    clock-frequency = <100000>;
    pinctrl-names = "default", "gpio";
    pinctrl-0 = <&pinctrl_i2c2>;
    pinctrl-1 = <&pinctrl_i2c2_gpio>;
    scl-gpios = <&gpio5 16 GPIO_ACTIVE_HIGH>;
    sda-gpios = <&gpio5 17 GPIO_ACTIVE_HIGH>;
    status = "okay";

    adv728x_mipi1: adv728x_mipi1@21 {
        status = "okay";
        compatible = "adi,adv7282-m";
        reg = <0x21>;
        pinctrl-names = "default";
        pinctrl-0 = <&pinctrl_csi1>;
        clocks = <&clk IMX8MM_CLK_CLKO1>;
        clock-names = "csi_mclk";
        csi_id = <0>;
        pwn-gpios = <&gpio5 12 GPIO_ACTIVE_HIGH>;
        rst-gpios = <&gpio1 13 GPIO_ACTIVE_HIGH>;
        mclk = <24000000>;
        mclk_source = <0>;
        port {
            adv728x_mipi1_ep: endpoint {
                remote-endpoint = <&mipi1_sensor_ep>;
            };
        };
    };
[...]
&mipi_csi_1 {
    #address-cells = <1>;
    #size-cells = <0>;
    status = "okay";
    port {
        mipi1_sensor_ep: endpoint@1 {
            remote-endpoint = <&adv728x_mipi1_ep>;
            data-lanes = <1>;
            csis-hs-settle = <13>;
            csis-clk-settle = <2>;
            csis-wclk;
        };

        csi1_mipi_ep: endpoint@2 {
            remote-endpoint = <&csi1_ep>;
        };
    };
};
[...]

 

 

 

Also added the following to mipi_csis_formats

 

 

{
		.code = MEDIA_BUS_FMT_UYVY8_2X8,
		.fmt_reg = MIPI_CSIS_ISPCFG_DOUBLE_CMPNT | MIPI_CSIS_ISPCFG_FMT_YCBCR422_8BIT,
		.data_alignment = 16,
}

 

 

 

The Video decoder seems to get initialized correctly according to dmesg

 

 

# dmesg | grep adv
[ 15.738849] adv7180 1-0021: chip found @ 0x21 (30a30000.i2c)
[ 15.769008] mxc_mipi-csi 32e30000.mipi_csi: Registered sensor subdevice: adv7180 1-0021

 

 

 

But when trying to capture, I get the following Error

 

 

# gst-launch-1.0 v4l2src device=/dev/video0 norm=PAL ! video/x-raw,format=UYVY,width=720,height=480,framerate=30/1 ! jpegenc ! avimux ! filesink location=mjpeg.avi
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock

(gst-launch-1.0:634): GStreamer-CRITICAL **: 14:53:19.617: range start is not smaller than end for `GstIntRange'
ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Device '/dev/video0' cannot capture at 720x480
Additional debug info:
gstv4l2object.c(3888): gst_v4l2_object_set_format_full (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:
Tried to capture at 720x480, but device returned size 720x240
Execution ended after 0:00:00.041957693
Setting pipeline to PAUSED ...
Setting pipeline to READY ...
Setting pipeline to NULL ...
Freeing pipeline ...

 

 

 

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,615件の閲覧回数
disennn
Contributor I
Hi, do you have fix for this?
0 件の賞賛
返信

2,179件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello kbch,


It looks like you have another format in stream, the module is ok: please get support formats:

$ v4l2-ctl -d /dev/video0 --list-formats-ext

and specify it in the pipeline:

$ gst-launch-1.0 v4l2src device=/dev/video0 ! <b>video/x-raw,format=YUY2,width=720, height=480,framerate=30/1</b> ! 'video/x-raw(memory:NVMM),format=NV12' ! overlaysink
0 件の賞賛
返信