iMX8M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M

2,293 Views
sales1
Contributor I

hello experts

I am using iMX8M mini(nitrogen8m mini) by boundary devices for my projects

this has LCD display and camera connected

I noticed that as soon as i touch few of the icons on the LCD screen the touch response is slow and the log messages show me

[  593.680084] alloc_contig_range: 23 callbacks suppressed
[  593.680089] alloc_contig_range: [98600, 98ee8) PFNs busy
[  593.691252] alloc_contig_range: [98700, 98fe8) PFNs busy
[  593.697671] alloc_contig_range: [98800, 990e8) PFNs busy
[  593.703557] alloc_contig_range: [98900, 991e8) PFNs busy
[  593.709410] alloc_contig_range: [98a00, 992e8) PFNs busy
[  593.715438] alloc_contig_range: [98b00, 993e8) PFNs busy

---------after sometime
[  813.320524] alloc_contig_range: 20 callbacks suppressed
[  813.320529] alloc_contig_range: [9d100, 9d9cb) PFNs busy
[  813.331983] alloc_contig_range: [9d200, 9dacb) PFNs busy
[  813.338066] alloc_contig_range: [9d200, 9dbcb) PFNs busy
[  813.344150] alloc_contig_range: [9ec00, 9f4cb) PFNs busy
[  813.350252] alloc_contig_range: [9ed00, 9f5cb) PFNs busy
[  813.363012] alloc_contig_range: [9ee00, 9f6cb) PFNs busy
[  813.369245] alloc_contig_range: [9ef00, 9f7cb) PFNs busy
[  813.375417] alloc_contig_range: [9f000, 9f8cb) PFNs busy
[  813.381611] alloc_contig_range: [9f100, 9f9cb) PFNs busy
[  813.387774] alloc_contig_range: [9f200, 9facb) PFNs busy

test scenario:

1) now the default value is cma=736M the LCD display is fine but the touch response is slow. and logcat messages show every time i touch a bunch of these messages alloc_contig_range: [9f200, 9facb) PFNs busy

what i have tried so far:

2) i changed the cma=1024M the LCD does not display anything and the kernel messages show some sort of crash.

is there are solution for this guys please let me know

Regards

Nick

0 Kudos
Reply
1 Reply

2,053 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Nick,

If you are using Nitrogen boards, you should directly ask to Boundary Devices at the link below:
https://boundarydevices.com/support/

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos
Reply