iMX8M two qspi issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX8M two qspi issue

1,467 次查看
weikeng-jimmy
Contributor III

Hi Sir,

Customer want to enable two chip (w25q64dw) , but QSPI_B always probe failed as beolw message.

# dmesg | grep -i spi
[ 2.084054] fsl-quadspi 30bb0000.qspi: w25q64dw (8192 Kbytes)
[ 2.091144] fsl-quadspi 30bb0000.qspi: unrecognized JEDEC id bytes: ff, ff, ff
[ 2.098393] fsl-quadspi 30bb0000.qspi: Freescale QuadSPI probe failed
[ 2.104945] fsl-quadspi: probe of 30bb0000.qspi failed with error -2

I.MX8M only support two planes in one die mode ?

标记 (1)
0 项奖励
回复
1 回复

1,333 次查看
art
NXP Employee
NXP Employee

Is the IOMUX configured correctly for the QSPI_B channel signals? Can you see any activity on the QSPI_B channel signals when trying to access it? Please check.

0 项奖励
回复