iMX8M Plus CC Controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M Plus CC Controller

652 Views
govind18
Contributor I

Hii,
We are developing the custom som based on the iMX8M plus processors with custom carrier board. In this, We have a requirement for USB1 OTG supported with ID pin. We have taken ID pin from GPIO1_IO4.

Due to board space constraint and ID Pin requirement we are planning to use HD3SS3220IRNH - TI (CC Controller with diff mux) in our design.

Please confirm whether i.mx8m plus supports HD3SS3220IRNH as OTG. Specifically for Flashing purpose whether this controller is supported?

0 Kudos
Reply
4 Replies

594 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @govind18 

The i.MX 8M Plus can be configured in system designs to work with the TI HD3SS3220 to implement a dual-role USB Type-C port; however, this device is not a Type-C controller that has been officially verified or supported by NXP‘s EVK. GPIO1_IO4 can be used as USB ID in Uboot/Linux and does not affect UUU programming. It is recommended that the HD3SS3220 be configured to UFP/Sink by default at power-on.

Best Regards,
Zhiming

0 Kudos
Reply

582 Views
ramkrish
Contributor I

Hi @Zhiming_Liu 

Could you please suggest any other tested CC controller that has ID pin Supported?

0 Kudos
Reply

540 Views
ramkrish
Contributor I

Hi @Zhiming_Liu Could you please suggest CC controller?

0 Kudos
Reply

530 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi 
On EVK board, the i.MX8MP is using  PTN5110NHQZ  as CC controller. Please refer the EVK design here.

Zhiming_Liu_0-1789018946469.png

 

https://www.nxp.com/design/design-center/development-boards-and-designs/8MPLUSLPD4-EVK

Best Regards,
Zhiming

0 Kudos
Reply