iMX8M Mini GPU Profiling

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M Mini GPU Profiling

3,521 Views
banhu
Contributor I

Hello, Linux 5.4.70_2.3.0 BSP is installed IMX8M Mini.  galcore.gpuProfiler=1 is set in u-boot and as well as export VIV_PROFILE=1 in Linux environment. With glmark2-es2-wayland, I can find the vpd files. 

~# ls -lh *.vpd
-rw-r--r-- 1 root root 128 Jul  1 09:23 vprofiler_838_1.vpd
-rw-r--r-- 1 root root 19M Jul  1 09:23 vprofiler_838_2.vpd

 However the GPU utilization in VPD Analyzer is always 0% when vpd file is loaded. That is obviously not true as glmark2-es2-wayland does use GPU for rendering. The same test on iMX8M Plus shows GPU load varying from 10% to 70%. Doesn't the iMX8M Mini's GPU GC7000NanoUltra support such profiling? Thanks!

imx8mm.png

 

0 Kudos
Reply
2 Replies

3,510 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello banhu,

 

Please take a look that If you put in uboot galcore.powerManagement=0, Sometime give you some data on vpd, however this feature is not available on GC7000Nano, It suppose to be fully supported in next release of the gpu driver, you can try the 5.10.35 BSP.

Regards

0 Kudos
Reply

3,501 Views
banhu
Contributor I

Hi @Bio_TICFSL , thanks for replying. I will try 5.10.35 BSP later. galcore.powerManagement=0 in -uboot doesn't generate GPU utilization data. 

0 Kudos
Reply