iMX8M Mini EVK LPDDR4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8M Mini EVK LPDDR4

1,898件の閲覧回数
tom_perman
Contributor III

Hi,

I have some questions regarding the iMX8M Mini EVK design, specifically the LPDDR4 sheet in SOM schematic "8MMINILPD4-CPU" and more general LPDDR4 questions. 


  • Why is there a 150R resistor termination on the DRAM_CK differential signals?
    • This isn't mentioned in the Hardware Design Guide, and hasn't been observed on LPDDR4 designs for other SoCs
  • What is the purpose of the DNP 10K resistors R123, R124, R121 & R122 on DRAM_CKE0/1 
  • The recommendation in the Hardware Design Guide is to use 85 Ohm differential controlled impedance for DDR DQS/CLK. However on other LPDDR4 designs these are routed at 100 Ohms. Why is this recommendation different from the standard used?

Thanks,

Tom 

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,664件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

   The i.MX8Mm design recommendations are result of working with the EVK design, therefore

some discrepancies may be observed here. Please try to meet the recent design recommendations.

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 件の賞賛
返信