I see in the latest yocto LF5.10.35_2.0.0
the default local has:
PACKAGE_CLASSES = "Package_deb"
EXTRA_IMAGE_FEATURES += "package-management"
It states somewhere that this makes it easy to pull in public Debian packages using the apt-get.
But I do not see any package feeds set up.
How do you set up package feeds and is it possible to point to some public repo to install packages a'la Ubuntu like?