iMX8 PLUS MIPI raw8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8 PLUS MIPI raw8

8,451件の閲覧回数
Creative
Contributor III

Hi
Our iMX8 PLUS platform
Our task is to get an image in RAW8 format (10, 12)
AR0521 sensor (4 lines MIPI)
I managed to integrate the driver for the sensor
And get a crooked image, the image is as if divided into 4 parts, the first two squares display the image of the image, the other two are just black.

The questions are as follows:
1) What changes need to be made to the MIPI (CSI) driver to get an image in RAW8 (10, 12)?
2) There is data on the MIPI bus, but there is no CLK, what could be the reason?

Any help would be helpful, thanks

0 件の賞賛
返信
6 返答(返信)

8,397件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Russel

 

In case of using 5.10.x version of BSP, recommended to try applying the attached BSP patch, verified with OV5640 sensor.

 

Best regards
igor

0 件の賞賛
返信

5,884件の閲覧回数
Olivia
Contributor I

Hello @igorpadykov ,

                    I am working same sensor with Y8 format with 6.1.36 version. Can i get a patch for both ISI and Sensor.

 

 

Regards,

Olivia

 

0 件の賞賛
返信

7,995件の閲覧回数
JesterOfHw
Contributor IV

this was solution to our issue that matched the below image OP added. no more side by side double and half full of NULL.

SOLUTION 

タグ(5)
0 件の賞賛
返信

8,310件の閲覧回数
chensam
Contributor I

Hi igorpadykov

Can you tell me which the BSP version of the attached BSP patch?

I using imx8mp-evk board with bsp version is 5.10.35, and want to get mipi ov5640 8 bit raw data.

0 件の賞賛
返信

8,427件の閲覧回数
Creative
Contributor III

Addition:
1) Image with lens attached (see below)
2) ar0521 - monochrome

Image from iOS.jpgImage from iOS.jpg

0 件の賞賛
返信

7,997件の閲覧回数
JesterOfHw
Contributor IV

I've run into this exact issue as well. was there a solution to this? 

EDIT: I tried the patch and it solved this issue for me.

0 件の賞賛
返信