iMX7s USB suspend (peripheral mode)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX7s USB suspend (peripheral mode)

2,592件の閲覧回数
lucas_lin
Contributor I

Hi,

I set USB OTG to peripheral mode and to run some USB test.

About the suspend mode test.

When the host enter S3, the device (iMX7s) shall enter suspend mode too.

But my device still stay in run mode.


My question is if usb driver received suspend signal from host, can it make whole system enter suspend mode (suspend to ram) or just itself will enter suspend mode?

Thank you for your help.

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

2,512件の閲覧回数
lucas_lin
Contributor I

Hi Bio,

Did you mean that when usb got suspend signal from host and enter suspend state, it will bring whole system enter suspend mode?
If yes, which configurations I need to set?
Because my EV-Board is always stay in run mode even the host already enter to S3.

Thank you.

0 件の賞賛
返信

2,512件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Sorry No, If you don´t tell the board to enter suspend mode it won´t enter.

0 件の賞賛
返信

2,512件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Lucas,

Yes, It will enter to suspend mode.

Regards

0 件の賞賛
返信