Hi All
The customer don't use MIPI and PCIe interface, but external have link decoupling capacitor, like as below schematic.
VDDD_1P0_CAP and VDDA_PHY_1P8 and VDD_1P2_CAP measurement voltage is 0 V.
Could you tell me VDDD_1P0_CAP and VDDA_PHY_1P8 and VDD_1P2_CAP don't pull down will have any concern?
Thanks.
已解决! 转到解答。
Hello,
Generally customers can use section 3.2 (Recommended connections for unused analog interfaces)
of i.MX7D Datasheet, Rev. 5, 07/2017, where the MIPI and PCIe supply pins are recommended to be
grounded.
It is possible to provide corresponding (correct) supply voltages for the MIPI and PCIe, when the modules
are not used.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
Generally customers can use section 3.2 (Recommended connections for unused analog interfaces)
of i.MX7D Datasheet, Rev. 5, 07/2017, where the MIPI and PCIe supply pins are recommended to be
grounded.
It is possible to provide corresponding (correct) supply voltages for the MIPI and PCIe, when the modules
are not used.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------