iMX6q Sabre AI GPIO wdt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6q Sabre AI GPIO wdt

1,615 Views
francescocamard
Contributor I

Hello All,

does this board have a specific GPIO that triggers a wdt (watch dog timer) event as reboot, boot loading fail or similar?

Thanks,

Francesco

Labels (1)
0 Kudos
Reply
7 Replies

1,382 Views
igorpadykov
NXP Employee
NXP Employee

Hi francesco

yes this is WDOG1_B signal on SPF-27142 p.9

Design files, including hardware schematics, layout files and BOM

SABRE|Automotive-Infotainment|i.MX6|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,382 Views
francescocamard
Contributor I

Hi Igor,

I had time now to probe this signal but it's not toggling when a reboot occurs, only when i detach the power.

I also probed (with oscillo) the:

  1. GPIO1_14 --> BOOT_COMPLETE
  2. TP7 --> Hi-Z_FOR_BOOT_B

and all have the same pattern. Could you suggest some signal as reboot indicator?

Thanks and Regards,

Francesco

0 Kudos
Reply

1,382 Views
igorpadykov
NXP Employee
NXP Employee

Hi Francesco

Table 100, Table 101 i.MX6DQ Datasheet (rev.4, 7/2015)

shows fixed after reset state of signals. So one can try to use

one pin (setting it to opposite state) as such indicator

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards

igor

0 Kudos
Reply

1,382 Views
francescocamard
Contributor I

Hi Igor,

any update?

Thanks & Regards,

Francesco

0 Kudos
Reply

1,382 Views
igorpadykov
NXP Employee
NXP Employee

Hi Francesco

I am afraid no message sent specific for wdt reset.

~igor

0 Kudos
Reply

1,382 Views
francescocamard
Contributor I

Hi Igor,

when a WDOG occurs ( I had two triggered events) do you know if any message is written into the dmesg (or some other log)?  Or only a reboot occurs?

Thanks,

Francesco

0 Kudos
Reply

1,382 Views
francescocamard
Contributor I

Hello Igor,

thanks for the answer. I saw the WDOG in the layout, is there any TP where I can solder a wire?

Regards,

Francesco

0 Kudos
Reply