iMX6q Kernel support HS200?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6q Kernel support HS200?

2,281 Views
disayin
Contributor I

Hi Sir,

I want to know whether  iMX6q kernel can support HS200? If the kernel can support HS200, which version is the kernel?

3 Replies

2,147 Views
igorpadykov
NXP Employee
NXP Employee

Hi yixiao

i.MX6Q does not support HS200 mode, it may be supported

by i.MX6SL which has upgraded uSDHC controller.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,147 Views
disayin
Contributor I

Sorry sir, you means Hardware of chip can't support HS200 mode?

0 Kudos
Reply

2,147 Views
igorpadykov
NXP Employee
NXP Employee

yes, right.

~igor

0 Kudos
Reply