iMX6ULLEVK start problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6ULLEVK start problem

ソリューションへジャンプ
5,241件の閲覧回数
zhangjinfei6688
Contributor II

My iMX6ULLEVK starting stop is in the starting kernel...;Later, I downloaded the kernel source code from the official website and copied the generated zImage and DTB files to the SD card.But the error will still be reported after startup:

 

EXT3-fs (mmcblk1p2): error: couldn't mount because of unsupported optional featu res (240)
EXT2-fs (mmcblk1p2): error: couldn't mount because of unsupported optional featu res (244)
EXT4-fs (mmcblk1p2): warning: mounting fs with errors, running e2fsck is recomme nded
EXT4-fs (mmcblk1p2): recovery complete
EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
VFS: Mounted root (ext4 filesystem) on device 179:2.
devtmpfs: mounted
Freeing unused kernel memory: 400K (8090e000 - 80972000)
INIT: version 2.88 booting
INIT: Entering runlevel: 5 /bin/sh: sym
/bin/sh: relocation error: /bin/sh: symbol rea,loc, version GLIBC_2.4 not define d in file libc.so.6 with link time reference
/bin/start_getty: line 5: 62 Segmentation fault /sbin/getty -L $1 $2
/bin/sh: relocation error: /bin/sh: symbol ex▒t, version GLIBC_2.4 not defined i n file libc.so.6 with link time reference
/bin/start_getty: line 5: 67 Segmentation fault /sbin/getty -L $1 $2
/bin/sh: relocation error: /bin/sh: symbol ex▒t, version GLIBC_2.4 not defined i n file libc.so.6 with link time reference
/bin/start_getty: line 5: 70 Segmentation fault /sbin/getty -L $1 $2
/bin/sh: relocation error: /bin/sh: symbol ex▒t, version GLIBC_2.4 not defined i n file libc.so.6 with link time reference
/bin/start_getty: line 5: 75 Segmentation fault /sbin/getty -L $1 $2
/bin/sh: relocation error: /bin/sh: symbol ex▒t, version GLIBC_2.4 not defined i n file libc.so.6 with link time reference
/bin/start_getty: line 5: 78 Segmentation fault /sbin/getty -L $1 $2
/bin/sh: relocation error: /bin/sh: symbol ex▒t, version GLIBC_2.4 not defined i

I think that is the problem that the root file system, so the mount to a host of NFS directory, set up: the setenv bootargs' root = / dev/NFS rw nfsroot XXX, XXX, XXX, XXX:. / Linux/NFS/rootfs IP = XXX XXX, XXX, XXX: : : : : : eth0: off ', problems still exist, same has been bothering me for a week, I am a novice, trouble ace to help me.I started it from the SD card as per IMX6ULLEVKHUG.

ラベル(3)
タグ(1)
0 件の賞賛
返信
1 解決策
5,082件の閲覧回数
zhangjinfei6688
Contributor II

hi,Tita wang

I've solved the problem.Use mfgtool to download uboot, kernel, DTB, rootfs again

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
5,082件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version of BSP are you using?

0 件の賞賛
返信
5,083件の閲覧回数
zhangjinfei6688
Contributor II

hi,Tita wang

I've solved the problem.Use mfgtool to download uboot, kernel, DTB, rootfs again

0 件の賞賛
返信
5,082件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Good news.

0 件の賞賛
返信
5,082件の閲覧回数
zhangjinfei6688
Contributor II

hi Rita Wang!

     After I received the development board, the power on the system starts up, and the system stops running in the starting kernel...;Later, I downloaded linux-imx-rel_imx_4.1.15_2.0.0_ga.tar source code, compiled, generated zImage and DTB, copied to micro SD card, and then started is the log as described above:

U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+g0ec2a01 (Nov 05 2016 - 01:13:31 -0500)

CPU: Freescale i.MX6ULL rev1.0 at 396MHz
CPU: Commercial temperature grade (0C to 95C) at 32C
Reset cause: POR
Board: MX6ULL 14x14 EVK
I2C: ready
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Display: TFT43AB (480x272)
Video: 480x272x24
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1 is current device
Net: FEC1
Normal Boot
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1 is current device
switch to partitions #0, OK
mmc1 is current device
reading boot.scr
** Unable to read file boot.scr **
reading zImage
5572576 bytes read in 298 ms (17.8 MiB/s)
Booting from mmc ...
reading imx6ull-14x14-evk.dtb
35921 bytes read in 61 ms (574.2 KiB/s)
Kernel image @ 0x80800000 [ 0x000000 - 0x5507e0 ]
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Using Device Tree in place at 83000000, end 8300bc50

Starting kernel ...

Booting Linux on physical CPU 0x0
Linux version 4.1.15 (y3fei@y3fei-PC) (gcc version 4.9.4 (Linaro GCC 4.9-2017.01) ) #1 SMP PREEMPT Sun Nov 17 14:34:08 CST 2019
CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Freescale i.MX6 ULL 14x14 EVK Board
Reserved memory: created CMA memory pool at 0x8c000000, size 320 MiB
Reserved memory: initialized node linux,cma, compatible id shared-dma-pool
Memory policy: Data cache writealloc
PERCPU: Embedded 12 pages/cpu @8bb32000 s16768 r8192 d24192 u49152
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk1p2 rootwait rw
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 180880K/524288K available (6875K kernel code, 320K rwdata, 2348K rodata, 392K init, 423K bss, 15728K reserved, 327680K cma-reserved, 0K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xa0800000 - 0xff000000 (1512 MB)
lowmem : 0x80000000 - 0xa0000000 ( 512 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.text : 0x80008000 - 0x80909edc (9224 kB)
.init : 0x8090a000 - 0x8096c000 ( 392 kB)
.data : 0x8096c000 - 0x809bc200 ( 321 kB)
.bss : 0x809bf000 - 0x80a28ff0 ( 424 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptible hierarchical RCU implementation.
Additional per-CPU info printed with stalls.
RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
NR_IRQS:16 nr_irqs:16 16
mxc_clocksource_init 24000000
Switching to timer-based delay loop, resolution 41ns
sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=240000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
/cpus/cpu@0 missing clock-frequency property
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x80008280 - 0x800082f0
Brought up 1 CPUs
SMP: Total of 1 processors activated (48.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
device-tree: Duplicate name in lcdif@021c8000, renamed to "display#1"
VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5
clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 8 bytes.
imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
imx6ul-pinctrl 2290000.iomuxc-snvs: initialized IMX pinctrl driver
mxs-dma 1804000.dma-apbh: initialized
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c i2c-0: IMX I2C adapter registered
i2c i2c-0: can't use DMA
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
PTP clock support registered
Advanced Linux Sound Architecture Driver Initialized.
Switched to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
imx rpmsg driver is registered.
Bus freq driver module loaded
futex hash table entries: 256 (order: 2, 16384 bytes)
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) ? 2001-2006 Red Hat, Inc.
fuse init (API version 7.23)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: Driver registered.
backlight supply power not found, using dummy regulator
21c8000.lcdif supply lcd not found, using dummy regulator
mxsfb 21c8000.lcdif: failed to find mxc display driver
Console: switching to colour frame buffer device 60x34
mxsfb 21c8000.lcdif: initialized
imx-sdma 20ec000.sdma: no event needs to be remapped
imx-sdma 20ec000.sdma: loaded firmware 3.3
imx-sdma 20ec000.sdma: initialized
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 18, base_baud = 5000000) is a IMX
console [ttymxc0] enabled
21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 235, base_baud = 5000000) is a IMX
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
fsl-quadspi 21e0000.qspi: n25q256a (32768 Kbytes)
20b4000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
libphy: fec_enet_mii_bus: probed
fec 20b4000.ethernet eth0: registered PHC device 0
2188000.ethernet supply phy not found, using dummy regulator
pps pps1: new PPS source ptp1
fec 2188000.ethernet eth1: registered PHC device 1
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
2184000.usb supply vbus not found, using dummy regulator
2184200.usb supply vbus not found, using dummy regulator
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
Mass Storage Function, version: 2009/09/11
LUN: removable file: (no medium)
no file given for LUN0
g_mass_storage ci_hdrc.0: failed to start g_mass_storage: -22
mousedev: PS/2 mouse device common for all mice
input: 20cc000.snvs:snvs-powerkey as /devices/platform/soc/2000000.aips-bus/20cc000.snvs/20cc000.snvs:snvs-powerkey/input/input0
input: iMX6UL TouchScreen Controller as /devices/platform/soc/2000000.aips-bus/2040000.tsc/input/input1
snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x/sz) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR SANYO protocol handler initialized
IR Sharp protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR XMP protocol handler initialized
pxp-v4l2 pxp_v4l2: initialized
imx2-wdt 20bc000.wdog: use WDOG_B to reboot.
imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
/soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified
sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified
sdhci-esdhc-imx 2194000.usdhc: could not get ultra high speed state, work on normal mode
sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
Key type dns_resolver registered
cpu cpu0: dev_pm_opp_get_opp_count: device OPP not found (-19)
mmc1: host does not support reading read-only switch, assuming write-enable
Registering SWP/SWPB emulation handler
mmc1: new high speed SDHC card at address 0001
snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)
mmcblk1: mmc1:0001 SD16G 14.5 GiB
mmcblk1: p1 p2
VSD_3V3: disabling
can-3v3: disabling
ALSA device list:
No soundcards found.
EXT3-fs (mmcblk1p2): error: couldn't mount because of unsupported optional features (240)
EXT2-fs (mmcblk1p2): error: couldn't mount because of unsupported optional features (244)
EXT4-fs (mmcblk1p2): warning: mounting fs with errors, running e2fsck is recommended
EXT4-fs (mmcblk1p2): recovery complete
EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
VFS: Mounted root (ext4 filesystem) on device 179:2.
devtmpfs: mounted
Freeing unused kernel memory: 392K (8090a000 - 8096c000)
INIT: version 2.88 booting
INIT: Entering runlevel: 5 /bin/sh: sym
/bin/sh: relocation error: /bin/sh: symbol rea,loc, version GLIBC_2.4 not defined in file libc.so.6 with link time reference
/sbin/getty: error while loading shared libraries: l?bm.so.6: cannot open shared object file: No such file or directory
/sbin/getty: error while loading shared libraries: l?bm.so.6: cannot open shared object file: No such file or directory
/bin/sh: relocation error: /bin/sh: symbol ex?t, version GLIBC_2.4 not defined in file libc.so.6 with link time reference
/sbin/getty: error while loading shared libraries: l?bm.so.6: cannot open shared object file: No such file or directory
/sbin/getty: error while loading shared libraries: l?bm.so.6: cannot open shared object file: No such file or directory
/sbin/getty: error while loading shared libraries: l?bm.so.6: cannot open shared object file: No such file or directory
/sbin/getty: error while loading shared libraries: l?bm.so.6: cannot open shared object file: No such file or directory
/bin/sh: relocation error: /bin/sh: symbol ex?t, version GLIBC_2.4 not defined in file libc.so.6 with link time reference
/sbin/getty: error while loading shared libraries: l?bm.so.6: cannot open shared object file: No such file or directory
/sbin/getty: error while loading shared libraries: l?bm.so.6: cannot open shared object file: No such file or directory
/sbin/getty: error while loading shared libraries: l?bm.so.6: cannot open shared object file: No such file or directory
/sbin/getty: error while loading shared libraries: l?bm.so.6: cannot open shared object file: No such file or directory
/bin/sh: relocation error: /bin/sh: symbol ex?t, version GLIBC_2.4 not defined in file libc.so.6 with link time reference
/sbin/getty: error while loading shared libraries: l?bm.so.6: cannot open shared object file: No such file or directory
/sbin/getty: error while loading shared libraries: l?bm.so.6: cannot open shared object file: No such file or directory
INIT: Id "1" respawning too fast: disabled for 5 minutes
/sbin/getty: error while loading shared libraries: l?bm.so.6: cannot open shared object file: No such file or directory
/bin/sh: relocation error: /bin/sh: symbol ex?t, version GLIBC_2.4 not defined in file libc.so.6 with link time reference
/sbin/getty: error while loading shared libraries: l?bm.so.6: cannot open shared object file: No such file or directory
/bin/sh: relocation error: /bin/sh: symbol ex?t, version GLIBC_2.4 not defined in file libc.so.6 with link time reference
/sbin/getty: error while loading shared libraries: l?bm.so.6: cannot open shared object file: No such file or directory
/bin/sh: relocation error: /bin/sh: symbol ex?t, version GLIBC_2.4 not defined in file libc.so.6 with link time reference
/sbin/getty: error while loading shared libraries: l?bm.so.6: cannot open shared object file: No such file or directory
/bin/sh: relocation error: /bin/sh: symbol ex?t, version GLIBC_2.4 not defined in file libc.so.6 with link time reference
/sbin/getty: error while loading shared libraries: l?bm.so.6: cannot open shared object file: No such file or directory
/bin/sh: relocation error: /bin/sh: symbol ex?t, version GLIBC_2.4 not defined in file libc.so.6 with link time reference
/sbin/getty: error while loading shared libraries: l?bm.so.6: cannot open shared object file: No such file or directory
/bin/sh: relocation error: /bin/sh: symbol ex?t, version GLIBC_2.4 not defined in file libc.so.6 with link time reference
INIT: Id "mxc0" respawning too fast: disabled for 5 minutes
INIT: no more processes left in this runlevel

0 件の賞賛
返信