iMX6ULL evaluation board NAND support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6ULL evaluation board NAND support

1,631件の閲覧回数
awong121
Contributor I

In the imX6ULL evaluation board schematic on the page for Flash there is a MTFC8GACAAAM on the lower left. It is not connected to anything as far as I can see. Am I right? I think it is just a footprint. Why is it there? I want to solder a BGA NAND flash to the board but this footprint seems to be not connected electrically to anything. i want to see whether I have missed anything. Thanks.

0 件の賞賛
返信
2 返答(返信)

1,623件の閲覧回数
Yuri
NXP Employee
NXP Employee

@awong121 

Hello,

   MTFC8GACAAAM is eMMC. According to section 2.6 (eMMC)of i.MX 6ULL EVK Board Hardware User's Guide:
The eMMC interface is connected to USDHC2 of i.MX 6ULL. It can support up to eMMC 4.5, the
eMMC device is not populated by default on the EVK board. To boot from eMMC, remove the Micro SD
socket and populate the eMMC device, and then change the boot device switch (SW601) settings
(OFF, ON, ON, OFF) as shown in Table 3 Additionally, the BOOT_CFG settings must be adjusted for
the specified eMMC device by exchanging the pull up/down resistors.


http://nxp.com/doc/imx6ullevkhug

    NAND on the EVK is mentioned as MT29F32G08CBADBW. Use section 2.8 (NAND flash) of the Guide
for more details.


Regards,
Yuri.

0 件の賞賛
返信

1,628件の閲覧回数
mike_nxp_commun
Contributor I

It's for TSOP-48 NAND. http://nxp.com/doc/imx6ullevkhug

0 件の賞賛
返信