iMX6ULL & iMX7D Audio Streaming Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6ULL & iMX7D Audio Streaming Issue

1,364件の閲覧回数
subbaiahnv
Contributor I
we are capturing microphone audio with iMX6ULL based board and sending to iMX7D based board over RTP protocol using g-streamer pipeline. Both the boards are using same codec.
 
We are seeing the packet loss at receving side iMX7D side. Whereas iMX7D capturing mic data and sending to iMX6ULL over RTP working fine.
 
If we record the mic data in iMX6ULL and copy the data to iMX7D then we are not seeing any issue. With this We are confident that there are no issues with the codec. Also the same codec working fine with ATMEL SAMA5D27 series processor.
 
We are facing the issue with NXP devices. What could be the issue. Kindly support.
 
Sender
root@imx6ull:~# gst-launch-1.0 -v alsasrc device=hw:0,0 ! audioconvert ! audioresample ! audio/x-raw, format=S16LE, channels=1, rate=44100 ! tcpclientsink host=192.168.0.134 port=5001
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Setting pipeline to PLAYING ...
New clock: GstAudioSrcClock
/GstPipeline:pipeline0/GstAlsaSrc:alsasrc0: actual-buffer-time = 200000
/GstPipeline:pipeline0/GstAlsaSrc:alsasrc0: actual-latency-time = 10000
Redistribute latency...
/GstPipeline:pipeline0/GstAlsaSrc:alsasrc0.GstPad:src: caps = audio/x-raw, rate=(int)44100, format=(string)S16LE, channels=(int)2, layout=(string)interleaved, channel-mask=(bitmask)0x0000000000000003
/GstPipeline:pipeline0/GstAudioConvert:audioconvert0.GstPad:src: caps = audio/x-raw, rate=(int)44100, format=(string)S16LE, channels=(int)2, layout=(string)interleaved, channel-mask=(bitmask)0x0000000000000003
/GstPipeline:pipeline0/GstAudioResample:audioresample0.GstPad:src: caps = audio/x-raw, rate=(int)44100, format=(string)S16LE, channels=(int)2, layout=(string)interleaved, channel-mask=(bitmask)0x0000000000000003
/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:src: caps = audio/x-raw, rate=(int)44100, format=(string)S16LE, channels=(int)2, layout=(string)interleaved, channel-mask=(bitmask)0x0000000000000003
/GstPipeline:pipeline0/GstTCPClientSink:tcpclientsink0.GstPad:sink: caps = audio/x-raw, rate=(int)44100, format=(string)S16LE, channels=(int)2, layout=(string)interleaved, channel-mask=(bitmask)0x0000000000000003
/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:sink: caps = audio/x-raw, rate=(int)44100, format=(string)S16LE, channels=(int)2, layout=(string)interleaved, channel-mask=(bitmask)0x0000000000000003
/GstPipeline:pipeline0/GstAudioResample:audioresample0.GstPad:sink: caps = audio/x-raw, rate=(int)44100, format=(string)S16LE, channels=(int)2, layout=(string)interleaved, channel-mask=(bitmask)0x0000000000000003
/GstPipeline:pipeline0/GstAudioConvert:audioconvert0.GstPad:sink: caps = audio/x-raw, rate=(int)44100, format=(string)S16LE, channels=(int)2, layout=(string)interleaved, channel-mask=(bitmask)0x0000000000000003
WARNING: from element /GstPipeline:pipeline0/GstAlsaSrc:alsasrc0: Can't record audio fast enough
Additional debug info:
../git/gst-libs/gst/audio/gstaudiobasesrc.c(841): gst_audio_base_src_create (): /GstPipeline:pipeline0/GstAlsaSrc:alsasrc0:
Dropped 28665 samples. This is most likely because downstream can't keep up and is consuming samples too slowly.
WARNING: from element /GstPipeline:pipeline0/GstAlsaSrc:alsasrc0: Can't record audio fast enough
Additional debug info:
../git/gst-libs/gst/audio/gstaudiobasesrc.c(841): gst_audio_base_src_create (): /GstPipeline:pipeline0/GstAlsaSrc:alsasrc0:
Dropped 22050 samples. This is most likely because downstream can't keep up and is consuming samples too slowly.
WARNING: from element /GstPipeline:pipeline0/GstAlsaSrc:alsasrc0: Can't record audio fast enough
Additional debug info:
../git/gst-libs/gst/audio/gstaudiobasesrc.c(841): gst_audio_base_src_create (): /GstPipeline:pipeline0/GstAlsaSrc:alsasrc0:
Dropped 51156 samples. This is most likely because downstream can't keep up and is consuming samples too slowly.
WARNING: from element /GstPipeline:pipeline0/GstAlsaSrc:alsasrc0: Can't record audio fast enough
Additional debug info:
../git/gst-libs/gst/audio/gstaudiobasesrc.c(841): gst_audio_base_src_create (): /GstPipeline:pipeline0/GstAlsaSrc:alsasrc0:
Dropped 48951 samples. This is most likely because downstream can't keep up and is consuming samples too slowly.
WARNING: from element /GstPipeline:pipeline0/GstAlsaSrc:alsasrc0: Can't record audio fast enough
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,342件の閲覧回数
subbaiahnv
Contributor I

Hi JorgeCas,

It is coming frequently for every 3 or 4 seconds capturing. There will be 50 msec data loss in the plying of IMX7D. 

0 件の賞賛
返信

1,346件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

How often does this warning appear?

All the time? At the beginning?

Best regards.

0 件の賞賛
返信