iMX6ULL adc calibration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6ULL adc calibration

1,619 次查看
barry_chen
Contributor I

Hi,dears,

I had the same problem as this little friend:

iMX6UL adc calibration fails 

My soc is iMx6uLL,but I tested at EVK board. EVK had this problem. So I think it has nothing to do with PCB.

Listed my config:

dts:

&adc1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_adc1>;
vref-supply = <&reg_vref_3v3>;
num-channels = <2>;
status = "okay";
};

pinctrl_adc1: adc1grp {
fsl,pins = <
MX6UL_PAD_GPIO1_IO08__GPIO1_IO08 0xb0
MX6UL_PAD_GPIO1_IO09__GPIO1_IO09 0xb0
>;
};

vf610_adc.c :
static const struct iio_chan_spec vf610_adc_iio_channels[] = {
   VF610_ADC_CHAN(9, IIO_VOLTAGE),
   VF610_ADC_CHAN(8, IIO_VOLTAGE),

};

#cat /sys/bus/iio/devices/iio\:device0/in_voltage8_raw
3976

In my PCBA board ,ADC_VREFH is OK,3.3V, but why cat out is 3976?

When I connected 1.8V, cat out value is 2233.

It's strange.

标签 (1)
0 项奖励
回复
1 回复

1,484 次查看
igorpadykov
NXP Employee
NXP Employee

Hi cheng

adc is not used in linux as it is used in sdk, so one can test it in sdk:

SDK2.2_iMX6ULL_WIN

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复