Hi all,
For a new project I need to interface 1GB RAM DD3L (2 x MT41K256M16TW-107:P) to iMX6ULL.
Is it possible? The BUS width is only 16bit so I suppose it is only possible to connect a single chip MT41K256M16TW-107:P.
Thanks,
Giacomo
Thank you Mrudang,
So can I consider that iMX6ULL is able to address 1GB RAM?
Regards,
Giacomo
Yes, it can work. https://community.nxp.com/thread/508998 You can see this.
Hi Giacomo,
i.MX6ULL based EVK "SCH-29634" provided part no# for both 512MB and 1GB.
Regards,
Mrudang
Hi Giacomo,
It is not possible for your suggested configuration. I suggest you use #MT41K512M16HA-125 (1 x16 bit) or equivalent.
https://www.micron.com/products/dram/ddr3-sdram/part-catalog/mt41k512m16ha-125-it
Let me know if you have any doubts
Regards,
Mrudang