iMX6UL uSDHC 1 or 2 interfaces

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6UL uSDHC 1 or 2 interfaces

2,007 次查看
johandeben
Contributor I

I'm wondering if the iMX6UL-1 has 1 or 2 uSDHC interfaces.

In the datasheet, I can find 2 interfaces.

But when using the Processor Expert for iMX6UL, I can only see 1 uSDHC interface.

So what is correct?

标签 (1)
0 项奖励
回复
2 回复数

1,749 次查看
Yuri
NXP Employee
NXP Employee

Hello,

    The Datasheet is correct - 2 uSDHC.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,749 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,

  See schematic page 7 SPF-28617_C1.pdf, please !
There are 2 uSDHC IPs in i.MX6ul, But SD2 signals are multiplexed with NAND Pads. So you had better refter to Reference Manual of i.MX6UL when you want to get PADs IOMUX mode.

Regards,

Weidong

0 项奖励
回复