iMX6UL uSDHC 1 or 2 interfaces

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6UL uSDHC 1 or 2 interfaces

1,968件の閲覧回数
johandeben
Contributor I

I'm wondering if the iMX6UL-1 has 1 or 2 uSDHC interfaces.

In the datasheet, I can find 2 interfaces.

But when using the Processor Expert for iMX6UL, I can only see 1 uSDHC interface.

So what is correct?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,710件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

    The Datasheet is correct - 2 uSDHC.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,710件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,

  See schematic page 7 SPF-28617_C1.pdf, please !
There are 2 uSDHC IPs in i.MX6ul, But SD2 signals are multiplexed with NAND Pads. So you had better refter to Reference Manual of i.MX6UL when you want to get PADs IOMUX mode.

Regards,

Weidong

0 件の賞賛
返信