iMX6UL Security Boot problem when linux kernel start

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6UL Security Boot problem when linux kernel start

1,697 Views
Eason_Lian
Contributor II

Hi Yuri,

    How to fix the problem?I have the same issue.

Thanks!

Eason

2 Replies

1,622 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Please provide console boot log.

It makes sense to create request

http://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,622 Views
Eason_Lian
Contributor II

Hi Yuri,

when I remove caam function from kernel,the system could start normal.Just for debug.

Thanks!

Eason