iMX6UL SPI transfer speedup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6UL SPI transfer speedup

1,236件の閲覧回数
IanCraig
Contributor II

Hi

I have a small TFT display connected to my iMX6UL board and I'm using the SPI interface to transfer the data. I have everything working but I'm looking to increase the data transfer speed. The SPI transfer is using DMA but when I look at the data transfer signals on a scope there is a significant gap between each 64-byte transfer. You can see this in the image below. A 64-byte transfer takes around 30uS and there is a 15uS gap before the next transfer takes place. This is all happening within the DMA transfer which is transferring  a total of 138240 bytes.

Does anybody have any ideas on how to decrease this gap?

spi transfer.jpg

Thanks

Ian

ラベル(4)
0 件の賞賛
返信
0 返答(返信)