iMX6SL Boot Options

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6SL Boot Options

1,398 Views
PotatoChip
Contributor I

Dear Community,

From "imx6 SoloLite quick start.pdf", page 9, it states setting SW3_7 for SD boot to 1 enable power cycle on power up and setting it to 0 with no power cycle.

From same page, it also states setting SW3_8, SW3_6, SW3_5 and SW3_4 depends on application.

I wonder if anyone can advise what they mean?

Best regards,

JJ

0 Kudos
Reply
1 Reply

1,292 Views
igorpadykov
NXP Employee
NXP Employee

Hi JJ

meaning can be found considering boot connections on p.13 spf-27452 i.MX6SL EVK schematic on :
Schematics (2)
Design files, including hardware schematics, Gerbers, and OrCAD files. (REV 1)
http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...
and description in Chapter 8 System Boot i.MX6SL Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SLRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply